2021-09-12 6:13 PM
the stm32programmer can connect, erase whole chip, but cannot program.
What I have done is to run example of SBSFU example (1 Image). I can see bootloader running. Then I try to erase the chip to program my other program.
I try to load the PCROP and secure section from my coworker's setting, but it does not allow me to change.
I attached all the stm32programmer logs.
May I know anyway can solve this lock program, or this device is actually locked
2021-09-14 4:47 AM
Hi @jiangpen ,
I think this may be related to the secure memory configuration, see appendix I in UM2262. Have you considered that?
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2021-09-22 7:14 AM
Hello @jiangpen
your option bytes have definitely not the good value.
Here is what you should get:
c:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=SWD -ob displ
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
ST-LINK SN : 0024001E3038511234333935
ST-LINK FW : V3J8M3
Board : STM32H7B3I-DK
Voltage : 3.29V
SWD freq : 24000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x480
Revision ID : Rev Z
Device name : STM32H7A/B
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x90
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x5200201c
Size : 308 Bytes
██████████████████████████████████████████████████ 100%
OPTION BYTES BANK: 0
Read Out Protection:
RDP : 0xAA (Level 0, no protection)
BOR Level:
BOR_LEV : 0x0 (reset level OFF)
User Configuration:
IWDG1_SW : 0x1 (Independent watchdog is controlled by software)
NRST_STOP : 0x1 (STOP mode on Domain 1 is entering without reset)
NRST_STBY : 0x1 (STANDBY mode on Domain 1 is entering without reset)
VDDMMC_HSLV : 0x0 (I/O speed optimization at low-voltage disabled)
IWDG_FZ_STOP : 0x1 (Independent watchdog is running in STOP mode)
IWDG_FZ_SDBY : 0x1 (Independent watchdog is running in STANDBY mode)
SECURITY : 0x0 (Security feature disabled)
VDDIO_HSLV : 0x0 (Product working in the full voltage range,I/O speed optimization at low-voltage disabled)
SWAP_BANK_OPT: 0x0 (after boot loading, no swap for user sectors)
Boot address Option Bytes:
BOOT_CM7_ADD0: 0x800 (0x8000000)
BOOT_CM7_ADD1: 0x1FF0 (0x1FF00000)
PCROP Protection:
PROT_AREA_START1: 0xFF (0x800FF00)
PROT_AREA_END1: 0x0 (0x80000FF)
DMEP1 : 0x1 (Flash Bank 1 PCROP zone is erased when RDP level regression (change from level 1 to 0) occurs)
PROT_AREA_START2: 0xFF (0x810FF00)
PROT_AREA_END2: 0x0 (0x81000FF)
DMEP2 : 0x1 (Flash Bank 2 PCROP zone is erased when RDP level regression (change from level 1 to 0) occurs)
Secure Protection:
SEC_AREA_START1: 0xFF (0x800FF00)
SEC_AREA_END1: 0x0 (0x80000FF)
DMES1 : 0x1 (Flash Bank 1 secure area is erased when RDP level regression (change from level 1 to 0) occurs)
SEC_AREA_START2: 0xFF (0x810FF00)
SEC_AREA_END2: 0x0 (0x81000FF)
DMES2 : 0x1 (Flash Bank 2 secure area is erased when RDP level regression (change from level 1 to 0) occurs)
DTCM RAM Protection:
ST_RAM_SIZE : 0x0 (2 KB)
Write Protection:
nWRP0 : 0x1 (Write protection not active)
nWRP1 : 0x1 (Write protection not active)
nWRP2 : 0x1 (Write protection not active)
nWRP3 : 0x1 (Write protection not active)
nWRP4 : 0x1 (Write protection not active)
nWRP5 : 0x1 (Write protection not active)
nWRP6 : 0x1 (Write protection not active)
nWRP7 : 0x1 (Write protection not active)
nWRP8 : 0x1 (Write protection not active)
nWRP9 : 0x1 (Write protection not active)
nWRP10 : 0x1 (Write protection not active)
nWRP11 : 0x1 (Write protection not active)
nWRP12 : 0x1 (Write protection not active)
nWRP13 : 0x1 (Write protection not active)
nWRP14 : 0x1 (Write protection not active)
nWRP15 : 0x1 (Write protection not active)
nWRP16 : 0x1 (Write protection not active)
nWRP17 : 0x1 (Write protection not active)
nWRP18 : 0x1 (Write protection not active)
nWRP19 : 0x1 (Write protection not active)
nWRP20 : 0x1 (Write protection not active)
nWRP21 : 0x1 (Write protection not active)
nWRP22 : 0x1 (Write protection not active)
nWRP23 : 0x1 (Write protection not active)
nWRP24 : 0x1 (Write protection not active)
nWRP25 : 0x1 (Write protection not active)
nWRP26 : 0x1 (Write protection not active)
nWRP27 : 0x1 (Write protection not active)
nWRP28 : 0x1 (Write protection not active)
nWRP29 : 0x1 (Write protection not active)
nWRP30 : 0x1 (Write protection not active)
nWRP31 : 0x1 (Write protection not active)
nWRP32 : 0x1 (Write protection not active)
nWRP33 : 0x1 (Write protection not active)
nWRP34 : 0x1 (Write protection not active)
nWRP35 : 0x1 (Write protection not active)
nWRP36 : 0x1 (Write protection not active)
nWRP37 : 0x1 (Write protection not active)
nWRP38 : 0x1 (Write protection not active)
nWRP39 : 0x1 (Write protection not active)
nWRP40 : 0x1 (Write protection not active)
nWRP41 : 0x1 (Write protection not active)
nWRP42 : 0x1 (Write protection not active)
nWRP43 : 0x1 (Write protection not active)
nWRP44 : 0x1 (Write protection not active)
nWRP45 : 0x1 (Write protection not active)
nWRP46 : 0x1 (Write protection not active)
nWRP47 : 0x1 (Write protection not active)
nWRP48 : 0x1 (Write protection not active)
nWRP49 : 0x1 (Write protection not active)
nWRP50 : 0x1 (Write protection not active)
nWRP51 : 0x1 (Write protection not active)
nWRP52 : 0x1 (Write protection not active)
nWRP53 : 0x1 (Write protection not active)
nWRP54 : 0x1 (Write protection not active)
nWRP55 : 0x1 (Write protection not active)
nWRP56 : 0x1 (Write protection not active)
nWRP57 : 0x1 (Write protection not active)
nWRP58 : 0x1 (Write protection not active)
nWRP59 : 0x1 (Write protection not active)
nWRP60 : 0x1 (Write protection not active)
nWRP61 : 0x1 (Write protection not active)
nWRP62 : 0x1 (Write protection not active)
nWRP63 : 0x1 (Write protection not active)
Best regards
Jocelyn