2022-08-19 5:28 AM
I worked on POC for X-CUBE-SBSFU in windows environment. It is all working fine without any issues.
Now the challenge is, we need to migrate SBSFU source to be compiled in Ubuntu Linux environment. I am struggling to do this, and getting lot of errors.
Can you please guide us to migrate SBSFU in ubuntu environment ??
@Fred Can you help on this ??
Logs
"../prebuild.sh" "../"
prepareimage with python script
python /home/nppdev/repos/SecureBoot/Middlewares/STM32_Secure_Engine/Utilities/KeysAndImages/prepareimage.py conf ..//../Inc/se_crypto_config.h
selected
create symbolic link postbuild.sh to .sh
arm-none-eabi-gcc -o "SECoreBin.elf" @"objects.list" -l:libSTM32CryptographicV3.1.1_STM32H7_GCC.a -mcpu=cortex-m7 -T"../STM32H753ZITx.ld" --specs=nosys.specs -Wl,-Map="SECoreBin.map" -Wl,--gc-sections -static -L../../../../../../../Middlewares/ST/STM32_Cryptographic/Fw_Crypto/STM32H7/Lib -Xlinker -L ../../../Linker_Common/STM32CubeIDE --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
arm-none-eabi-gcc: error: ./Application/Startup/se_key.o: No such file or directory
arm-none-eabi-gcc: error: ./Application/User/data_init.o: No such file or directory
arm-none-eabi-gcc: error: ./Application/User/se_crypto_bootloader.o: No such file or directory
arm-none-eabi-gcc: error: ./Application/User/se_low_level.o: No such file or directory
arm-none-eabi-gcc: error: ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_crc.o: No such file or directory
arm-none-eabi-gcc: error: ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_crc_ex.o: No such file or directory
arm-none-eabi-gcc: error: ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_flash.o: No such file or directory
arm-none-eabi-gcc: error: ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_flash_ex.o: No such file or directory
arm-none-eabi-gcc: error: ./Middlewares/STM32_Secure_Engine/se_callgate.o: No such file or directory
arm-none-eabi-gcc: error: ./Middlewares/STM32_Secure_Engine/se_crypto_common.o: No such file or directory
arm-none-eabi-gcc: error: ./Middlewares/STM32_Secure_Engine/se_exception.o: No such file or directory
arm-none-eabi-gcc: error: ./Middlewares/STM32_Secure_Engine/se_fwimg.o: No such file or directory
arm-none-eabi-gcc: error: ./Middlewares/STM32_Secure_Engine/se_startup.o: No such file or directory
arm-none-eabi-gcc: error: ./Middlewares/STM32_Secure_Engine/se_user_application.o: No such file or directory
arm-none-eabi-gcc: error: ./Middlewares/STM32_Secure_Engine/se_utils.o: No such file or directory
arm-none-eabi-gcc: error: ../../../Linker_Common/STM32CubeIDE: No such file or directory
makefile:66: recipe for target 'SECoreBin.elf' failed
make[1]: *** [SECoreBin.elf] Error 1
makefile:59: recipe for target 'all' failed
2022-08-19 5:54 AM
STM32CubeIDE is available for Linux.
STM32CubeIDE - Integrated Development Environment for STM32 - STMicroelectronics
I do not have a Linux machine but I guess that the CubeIDE project should work with the tool in Linux.
Or are you using command lines ?
2022-08-19 6:03 AM
Yes @Fred We are using command line, through MAKE file compilation.
We already had STM Binary generated with Makefile environment in ubuntu environent. So now we are trying to integrate SBSFU with same SDK.
Can you please help on this ?? if any sample project exist with.
2022-08-19 6:54 AM
I guess your problem is the way you invoke prebuild and postbuild.
Maybe you did a copy/paste from the IDE steps ?
These commands are supposed to be run from the PROJECT folder.
With your make infrastructure, I guess it is invoked from another place.
So, you must update the paths.
The paths in the IDE steps are relative to PROJECT so probably the STM32CubeIDE folder
2022-08-22 11:29 PM
I have taken care about the paths. But still something issues with Python scripts running in Linux environment.
I am debugging those, need to check.