cancel
Showing results for 
Search instead for 
Did you mean: 

Work with FSMC and two devices, problems with choosing one device

vik1970va
Associate II

Hello,

My program uses two FSMC_Bank1 for the tft screen and memory (62WV51216ALL), NORSRAM3 is used for memory and NORSRAM4 for the screen, a problem has been identified that when accessing NORSRAM3 (memory), the CS signal (FSMC_NE3) goes low and remains so permanently. The same thing happens with the signal for the CS screen (FSMC_NE4) and when garbage from points are written to the memory on the screen. How can I return the CS signals to their normal position after accessing the right data source?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

At this point I'm out of ideas.

You may want to try to ask for help ST directly through the web support form.

JW

View solution in original post

12 REPLIES 12
vik1970va
Associate II

STM32F407ZET

init SRAM

  readWriteTiming.FSMC_AddressSetupTime = 0x0F;	 
  readWriteTiming.FSMC_AddressHoldTime = 0x02;	
  readWriteTiming.FSMC_DataSetupTime = 0x0F;		 	 
  readWriteTiming.FSMC_BusTurnAroundDuration = 0x00;
  readWriteTiming.FSMC_CLKDivision = 0x00;
  readWriteTiming.FSMC_DataLatency = 0x00;
  readWriteTiming.FSMC_AccessMode = FSMC_AccessMode_B;	 
    
 
 
  FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM3;
  FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable; 
  FSMC_NORSRAMInitStructure.FSMC_MemoryType =FSMC_MemoryType_SRAM;// FSMC_MemoryType_SRAM;  //SRAM   
  FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b;
  FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode =FSMC_BurstAccessMode_Disable;// FSMC_BurstAccessMode_Disable; 
  FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;
  FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait=FSMC_AsynchronousWait_Disable;
  FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable;   
  FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState;  
  FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;	
  FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable;  
  FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Enable;
  FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable;  
  FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &readWriteTiming;
  FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &readWriteTiming;
  FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure);  
 
 	FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM3, ENABLE);  // BANK3	

init TFT

readWriteTiming.FSMC_AddressSetupTime = 0XF;	 // 1/168M=6ns*16=96ns	
  readWriteTiming.FSMC_AddressHoldTime = 0x00;	 
  readWriteTiming.FSMC_DataSetupTime = 24;			//6*25=150ns
  readWriteTiming.FSMC_BusTurnAroundDuration = 0x00;
  readWriteTiming.FSMC_CLKDivision = 0x00;
  readWriteTiming.FSMC_DataLatency = 0x00;
  readWriteTiming.FSMC_AccessMode = FSMC_AccessMode_A;	
    
 
	writeTiming.FSMC_AddressSetupTime =8;	      //Ö˜Ö·HCLK =48ns 
  writeTiming.FSMC_AddressHoldTime = 0x00;			
  writeTiming.FSMC_DataSetupTime = 8;		 //HCLK=54ns
  writeTiming.FSMC_BusTurnAroundDuration = 0x00;
  writeTiming.FSMC_CLKDivision = 0x00;
  writeTiming.FSMC_DataLatency = 0x00;
  writeTiming.FSMC_AccessMode = FSMC_AccessMode_A;	
 
 
  FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM4;
  FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable; 
  FSMC_NORSRAMInitStructure.FSMC_MemoryType =FSMC_MemoryType_SRAM;// FSMC_MemoryType_SRAM;  //SRAM   
  FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b;
  FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode =FSMC_BurstAccessMode_Disable;// FSMC_BurstAccessMode_Disable; 
  FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low;
	FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait=FSMC_AsynchronousWait_Disable; 
  FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable;   
  FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState;  
  FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable;	
  FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable;   
  FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Enable; 
  FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable; 
  FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &readWriteTiming;
  FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &writeTiming; 
 
  FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure); 
 
  FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM4, ENABLE);  // BANK1 

Read out and check/post content of FSMC registers.

JW

vik1970va
Associate II

По�?ле запи�?и в пам�?ть

0690X00000Bwk1AQAR.png

This looks to be OK, I don't see anything obviously wrong here.

If you use the two peripherals separately (i.e. initialize only one of them in FSMC) they work OK?

Try to disable Bank1.

JW

vik1970va
Associate II

Hello,

when one of the devices is turned off, the behavior of the CS (NE3 or NE4) signals becomes normal. disconnected separately the memory on the NE 4 logical analyzer; SWITCHED NORMALLY; turned off the screen (by setting comments on the screen); NE 3 switching is normal (attachment). The combined operation of the screen and memory causes a single change in the signal from 1 -> 0 at the outputs of NE 3 and NE 4

0690X00000BwlsPQAR.png

vik1970va
Associate II

Changed the initialization order, at the beginning of the screen then the memory. The screen selection signal NE 4 now works fine. BUT the memory selection signal does not work. In the attachment, the screen from the moment the microcontroller resets.0690X00000BwltDQAR.png

Maybe something is wrong with the memory access? I give all the pieces of the appeal code:

void fsmc_sram_test_1(void)
{   u16 temp=0;
    fsmc_sram_test_write(0x0000,0xBBAA);
    temp=fsmc_sram_test_read(0X0000);
    LCD_ShowxNum(60,190,temp,6,16,0);
    printf("Data SINGL:%x\r\n",temp);
}
/*****************************************************/
void FSMC_SRAM_WriteBuffer(u16* pBuffer,u32 WriteAddr,u32 n)
{
	for(;n!=0;n--)  
	{										    
		*(vu16*)(Bank1_SRAM3_ADDR+WriteAddr)=*pBuffer;	  
		WriteAddr++;
		pBuffer++;
	}    
}																			    
/*****************************************************/
void FSMC_SRAM_ReadBuffer(u16* pBuffer,u32 ReadAddr,u32 n)
{
	for(;n!=0;n--)  
	{											    
		*pBuffer++=*(vu16*)(Bank1_SRAM3_ADDR+ReadAddr);    
		ReadAddr++;
	}     
} 
/*****************************************************/
void fsmc_sram_test_write(u32 addr,u16 data)
{			   
	FSMC_SRAM_WriteBuffer(&data,addr,1);
}
/*****************************************************/
u16 fsmc_sram_test_read(u32 addr)
{
	u16 data;
	FSMC_SRAM_ReadBuffer(&data,addr,1);
	return data;
}

vik1970va
Associate II

Compulsory measures to return the signal have no effect :(

    *(vu16*)(Bank1_SRAM3_ADDR+0x0000)=0xBBAA; 
 GPIO_PinAFConfig(GPIOG,GPIO_PinSource10,GPIO_AF_RTC_50Hz); 
 GPIO_SetBits(GPIOG, GPIO_Pin_10);
 GPIO_PinAFConfig(GPIOG,GPIO_PinSource10,GPIO_AF_FSMC); 

In the simulator, everything is fine and in the iron there is no reaction to these actions.

Did you try to disable FSMC Bank1?

JW

vik1970va
Associate II

I do not understand why disable FSMC Bank1?

I turned off the devices one at a time and the selection line began to work in both cases. The collaboration of the devices is incorrect, but turning off FSMC Bank1 how will I work with a memory chip and a screen? Separately, port Port G -> pin 10 switches normally without problems.