2022-02-16 11:20 AM
I measure the execution time of a function by putting the toggle of a digital output and the function call into a cycle and measuring the period of the square wave at the digital output with an oscilloscope. The execution time is half a period.
To test the procedure, I used instead of the function a dummy code (see main function in the annex execution_time_main.c) where the cnt_max parameter allows me to vary the amount of code to execute.
The measured periods are visible in the attachment CRAZY_TIMES.jpg
I do not understand why both with the ARM V5 and V6 compiler in Keil uVision the trend of the periods is that shown in the attachment CRAZY_TIMES.jpg
Thanks
2022-02-22 05:22 AM
I don't have much "ARM experience" (more with AVRs & FPGAs), anyway, that behavior is really strange.
Maybe somehow the debugging is kinda intrusive, always checking the volatile variable?
2022-02-22 06:28 AM
The M7 pipeline is considerably more complex than a PIC or 68000 which leads to things like this. You have 7 wait states and if the processor needs to load two different pages, it will take some time. You can't get away with the simplicity of a constant X cycles per instruction when you're running at several hundred MHz. Things are exacerbated when your code is otherwise so short. Enabling ART Accelerator may eliminate this effect entirely, would be interesting to see.
2022-02-22 07:14 AM
I had similar problems without using the debugger, but measuring times by toggling a digital output and measuring the period with an oscilloscope
For example, consider the following code
#include "stm32f767xx.h"
void test_function (uint32_t iterations);
void initialize (void);
int main (void)
{
volatile uint32_t system_core_clock_for_watch = SystemCoreClock; // @1
__disable_irq();
initialize();
for (;;)
{
GPIOB->ODR ^= GPIO_ODR_OD10; // Toggle PB10
test_function(1000000UL);
}
return 0;
}
void test_function (uint32_t iterations)
{
volatile uint32_t cnt = 0;
/* Dummy code */
while (cnt < iterations)
{
cnt++;
}
}
void initialize (void)
{
volatile uint8_t cnt = 0; /* NOTE. cnt is only used to generate a small
delay. volatile ensures that compiler optimizations don't delete the
delay. */
/*--------------------------------------------------------------------------
* Configure PB10 (CN10.32 in NUCLEO-F767ZI) as DO
*------------------------------------------------------------------------*/
/* Enable IO port B clock */
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOBEN;
/* Small delay.
NOTE. From RM0410 rev 4 par par 5.2.12.
"Just after enabling the clock for a peripheral, software must wait for
a 2 peripheral clock cycles delay before accessing the peripheral
registers."
Port B is on AHB bus and AHB bus frequency is equal to HCLK frequency
that is equal to 216 MHz.*/
cnt = 0;
while (cnt < 100)
{
cnt++;
}
/* Configure MODER10 = 01b <==> General purpose output mode */
GPIOB->MODER &= ~GPIO_MODER_MODER10;
GPIOB->MODER |= (0 * GPIO_MODER_MODER10_1) | (1 * GPIO_MODER_MODER10_0);
/* Configure OSPEEDR10 = 00b <==> low speed */
GPIOB->OSPEEDR &= ~GPIO_OSPEEDR_OSPEEDR10;
GPIOB->OSPEEDR |= (0 * GPIO_OSPEEDR_OSPEEDR10_1) |
(0 * GPIO_OSPEEDR_OSPEEDR10_0);
}
Period measured with oscilloscope of signal at PB10 digital output is 687.7 ms
If you delete line 10
volatile uint32_t system_core_clock_for_watch = SystemCoreClock; // @1
the period becomes 1.892 s (x 2.75)
2022-02-22 07:51 AM
In my original problem, the clock was at 216 MHz and consequently the wait states were actually 7. Now the clock is at 16 MHz and there were no wait states. See tab 7 in the reference manual RM0410 rev 4 below..
2022-02-22 10:47 AM
Don't look to enable the MCU side caching either.
The CM7 is super-scaler, so how the underlying fetch mechanics and pairing works could account for some meta-stability issues in timing. These days I tend to focus on algorithmic improvements, rather than instruction level stuff, although obviously the longer the pipeline, the more impact stalls create, along with register dependency chains.
I don't think it's like the 68K where I can annotate timings directly into the disassembly listings, and get huge wins by instruction selection..
/**
* @brief CPU L1-Cache enable.
* @param None
* @retval None
*/
static void CPU_CACHE_Enable(void)
{
/* Enable I-Cache */
SCB_EnableICache();
/* Enable D-Cache */
SCB_EnableDCache();
}
2022-02-23 05:50 AM
Hi @Tesla DeLorean (Customer), @KiptonM (Customer), @TDK (Customer) and @LCE (Customer)
Tesla DeLorean is right 🙂
I tried to enable the cache and almost all the previous anomalies disappeared. The only "anomaly" left is the one reported on February 16, 2022 at 11:20 AM (I do not understand why ... test case 8 to 9 cnt_max go from 8000 to 9000 (increases) and period go from 485 us to 454 us (decreases)! ). Likely, as already said by you, could be the compiler rearranging things based on the compiled value.
Are there any reasons for deciding not to enable the cache?
2022-02-27 06:25 AM
Hi @Tesla DeLorean (Customer), @KiptonM (Customer), @TDK (Customer) and @LCE (Customer)
Thank you all for the time you have dedicated to me.