why can't program FLASH when FLASH all bit is 1?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-12 11:04 PM
I use STM32L431, it only possible to program double word, I want program a new data to FLASH if the 64 bits all is '1' in FLASH, otherwise, if the 64 bits is not all '1', I erase it first before program. But when I program a 0xffffffffffffffff to the 64 bits and then need to program a new data(for example: 0x1122334455667788), it fail to program.
void Flash_Test(void)
{
uint32_t startAddr = 0x0801C000;
HAL_StatusTypeDef status;
FLASH_EraseInitTypeDef EraseInitStruct;
uint32_t pageErr;
​
printf("erase one page\r\n");
/*erase one page*/
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES;
EraseInitStruct.Banks = GetBank(startAddr);
EraseInitStruct.Page = GetPage(startAddr);
EraseInitStruct.NbPages = 1;
status = HAL_FLASHEx_Erase(&EraseInitStruct, &pageErr);
HAL_FLASH_Lock();
if (status != HAL_OK)
return;
​
printf("before write 0xff to one page\r\n");
for (int i = 0; i < 2048; i += 4)
{
printf("%x ", *(volatile uint32_t*)(startAddr + i));
}
printf("\r\n");
​
/*write 0xff to one page*/
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
for (int i = 0; i < 2048; i += 8)
{
status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, startAddr + i, 0xffffffffffffffff);
if (status != HAL_OK)
{
printf("Fail to write all pages!\r\n");
break;
}
}
HAL_FLASH_Lock();
​
printf("after write 0xff to one page\r\n");
for (int i = 0; i < 2048; i += 4)
{
printf("%x ", *(volatile uint32_t*)(startAddr + i));
}
printf("\r\n");
​
printf("write 0xff\r\n");
/*write 8 bytes*/
HAL_FLASH_Unlock();
__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);
status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, startAddr, 0xffffffffffffffff);
if (status != HAL_OK)
{
printf("Fail to write 8 bytes!\r\n");
}
HAL_FLASH_Lock();
}
Run this sample code, it will print "Fail to write 8 bytes".
Possible to program 1 to 0 and can't program 0 to 1 is FLASH's feature. In this case, even if all the bits is '1' in FLASH, HAL_FLASH_Program still return HAL_ERROR. Why?
Thanks!
Solved! Go to Solution.
- Labels:
-
Flash
-
STM32L4 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-13 8:00 AM
Zzhou.2:
waclawek.jan's comment regarding the "hidden ECC bits getting programmed with a non-FF value" did not mean to imply that they were programmed incorrectly; indeed, the value programmed is correct -- that is, reading back the 0xFFFFFFFF will not result in a double-bit error (ECCD flag). What it means when the ECC bits are programmed to a non-FF value is that the corresponding STM32 Flash location is no longer alterable. In other words, when the device is erased, each 64-bits of Flash data and the associated 8 ECC bits all contain ''1' . This represents something of an "impossible" condition, since the ECC bits for a 64-bit value of "all FFs" is NOT itself 0xFF. You can perhaps understand this as being a specific condition rather than just one of many value settings. In any case, each of these '1's can be programmed to a '0' using the Flash write procedure, but any '0's cannot be programmed back to '1' -- they can only be erased to achieve that change. So, if you take a double-word Flash location that already contains 64 bits of '1's and perform a Flash write of (0xFFFFFFFF, 0xFFFFFFFF), it results in the same value but a different condition: that is, the 8 ECC bits will have changed. And once you've changed those, you cannot change them back. So, the writing of even a (0xFFFFFFFF,0xFFFFFFFF) will result in some '0' bits (in the corresponding ECC location), which will prevent you from being able to re-write that location. So, the error you should be getting when you try is not ECCD, but rather simply that the location could not be re-written.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-13 12:20 AM
The 'L4 FLASH has ECC. When you program 0xFFFFFFFFFFFFFFFF, the hidden ECC byte gets programmed to a non-FF value, this prevents further programming.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-13 1:30 AM
But the variable pFlash.ErrorCode=0xa8 in function FLASH_WaitForLastOperation​,not detect the flag FLASH_FLAG_ECCD.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-13 2:17 AM
I don't know what are those values you mention, I don't use Cube. You may want to talk in terms of register flags as given by the Reference Manual.
I suspect the dedicated ECCD error occurs only when you *read* from a FLASH position with mismatched ECC.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-13 8:00 AM
Zzhou.2:
waclawek.jan's comment regarding the "hidden ECC bits getting programmed with a non-FF value" did not mean to imply that they were programmed incorrectly; indeed, the value programmed is correct -- that is, reading back the 0xFFFFFFFF will not result in a double-bit error (ECCD flag). What it means when the ECC bits are programmed to a non-FF value is that the corresponding STM32 Flash location is no longer alterable. In other words, when the device is erased, each 64-bits of Flash data and the associated 8 ECC bits all contain ''1' . This represents something of an "impossible" condition, since the ECC bits for a 64-bit value of "all FFs" is NOT itself 0xFF. You can perhaps understand this as being a specific condition rather than just one of many value settings. In any case, each of these '1's can be programmed to a '0' using the Flash write procedure, but any '0's cannot be programmed back to '1' -- they can only be erased to achieve that change. So, if you take a double-word Flash location that already contains 64 bits of '1's and perform a Flash write of (0xFFFFFFFF, 0xFFFFFFFF), it results in the same value but a different condition: that is, the 8 ECC bits will have changed. And once you've changed those, you cannot change them back. So, the writing of even a (0xFFFFFFFF,0xFFFFFFFF) will result in some '0' bits (in the corresponding ECC location), which will prevent you from being able to re-write that location. So, the error you should be getting when you try is not ECCD, but rather simply that the location could not be re-written.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-13 8:08 AM
You get to program the cells ONCE, for the 0xFFFFFFFFF, 0xFFFFFFFFF case opt not to write them the first time around
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-15 3:22 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-10-15 3:22 PM
@GCord.1​ thanks for the exhaustive explanation.
Jan