cancel
Showing results for 
Search instead for 
Did you mean: 

why can't program FLASH when FLASH all bit is 1?

Zzhou.2
Associate

I use STM32L431, it only possible to program double word, I want program a new data to FLASH if the 64 bits all is '1' in FLASH, otherwise, if the 64 bits is not all '1', I erase it first before program. But when I program a 0xffffffffffffffff to the 64 bits and then need to program a new data(for example: 0x1122334455667788), it fail to program.

void Flash_Test(void)

{

uint32_t startAddr = 0x0801C000;

HAL_StatusTypeDef status;

FLASH_EraseInitTypeDef EraseInitStruct;

uint32_t pageErr;

​

printf("erase one page\r\n");

/*erase one page*/

HAL_FLASH_Unlock();

__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR); 

EraseInitStruct.TypeErase  = FLASH_TYPEERASE_PAGES;

EraseInitStruct.Banks    = GetBank(startAddr);

EraseInitStruct.Page    = GetPage(startAddr);

EraseInitStruct.NbPages   = 1;

status = HAL_FLASHEx_Erase(&EraseInitStruct, &pageErr);

HAL_FLASH_Lock();

if (status != HAL_OK)

return;

​

printf("before write 0xff to one page\r\n");

for (int i = 0; i < 2048; i += 4)

{

printf("%x ", *(volatile uint32_t*)(startAddr + i));

}

printf("\r\n");

​

/*write 0xff to one page*/

HAL_FLASH_Unlock();

__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);

for (int i = 0; i < 2048; i += 8)

{

status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, startAddr + i, 0xffffffffffffffff);

if (status != HAL_OK)

{

printf("Fail to write all pages!\r\n");

break;

}

}

HAL_FLASH_Lock();

​

printf("after write 0xff to one page\r\n");

for (int i = 0; i < 2048; i += 4)

{

printf("%x ", *(volatile uint32_t*)(startAddr + i));

}

printf("\r\n");

​

printf("write 0xff\r\n");

/*write 8 bytes*/

HAL_FLASH_Unlock();

__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);

status = HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, startAddr, 0xffffffffffffffff);

if (status != HAL_OK)

{

printf("Fail to write 8 bytes!\r\n");

}

HAL_FLASH_Lock();

}

Run this sample code, it will print "Fail to write 8 bytes".

Possible to program 1 to 0 and can't program 0 to 1 is FLASH's feature. In this case, even if all the bits is '1' in FLASH, HAL_FLASH_Program still return HAL_ERROR. Why?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Zzhou.2:

waclawek.jan's comment regarding the "hidden ECC bits getting programmed with a non-FF value" did not mean to imply that they were programmed incorrectly; indeed, the value programmed is correct -- that is, reading back the 0xFFFFFFFF will not result in a double-bit error (ECCD flag). What it means when the ECC bits are programmed to a non-FF value is that the corresponding STM32 Flash location is no longer alterable. In other words, when the device is erased, each 64-bits of Flash data and the associated 8 ECC bits all contain ''1' . This represents something of an "impossible" condition, since the ECC bits for a 64-bit value of "all FFs" is NOT itself 0xFF. You can perhaps understand this as being a specific condition rather than just one of many value settings. In any case, each of these '1's can be programmed to a '0' using the Flash write procedure, but any '0's cannot be programmed back to '1' -- they can only be erased to achieve that change. So, if you take a double-word Flash location that already contains 64 bits of '1's and perform a Flash write of (0xFFFFFFFF, 0xFFFFFFFF), it results in the same value but a different condition: that is, the 8 ECC bits will have changed. And once you've changed those, you cannot change them back. So, the writing of even a (0xFFFFFFFF,0xFFFFFFFF) will result in some '0' bits (in the corresponding ECC location), which will prevent you from being able to re-write that location. So, the error you should be getting when you try is not ECCD, but rather simply that the location could not be re-written.

View solution in original post

7 REPLIES 7
waclawek.jan
Super User

The 'L4 FLASH has ECC. When you program 0xFFFFFFFFFFFFFFFF, the hidden ECC byte gets programmed to a non-FF value, this prevents further programming.

JW

But the variable pFlash.ErrorCode=0xa8 in function FLASH_WaitForLastOperation​,not detect the flag FLASH_FLAG_ECCD.

waclawek.jan
Super User

I don't know what are those values you mention, I don't use Cube. You may want to talk in terms of register flags as given by the Reference Manual.

I suspect the dedicated ECCD error occurs only when you *read* from a FLASH position with mismatched ECC.

JW

Zzhou.2:

waclawek.jan's comment regarding the "hidden ECC bits getting programmed with a non-FF value" did not mean to imply that they were programmed incorrectly; indeed, the value programmed is correct -- that is, reading back the 0xFFFFFFFF will not result in a double-bit error (ECCD flag). What it means when the ECC bits are programmed to a non-FF value is that the corresponding STM32 Flash location is no longer alterable. In other words, when the device is erased, each 64-bits of Flash data and the associated 8 ECC bits all contain ''1' . This represents something of an "impossible" condition, since the ECC bits for a 64-bit value of "all FFs" is NOT itself 0xFF. You can perhaps understand this as being a specific condition rather than just one of many value settings. In any case, each of these '1's can be programmed to a '0' using the Flash write procedure, but any '0's cannot be programmed back to '1' -- they can only be erased to achieve that change. So, if you take a double-word Flash location that already contains 64 bits of '1's and perform a Flash write of (0xFFFFFFFF, 0xFFFFFFFF), it results in the same value but a different condition: that is, the 8 ECC bits will have changed. And once you've changed those, you cannot change them back. So, the writing of even a (0xFFFFFFFF,0xFFFFFFFF) will result in some '0' bits (in the corresponding ECC location), which will prevent you from being able to re-write that location. So, the error you should be getting when you try is not ECCD, but rather simply that the location could not be re-written.

You get to program the cells ONCE, for the 0xFFFFFFFFF, 0xFFFFFFFFF case opt not to write them the first time around

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

@GCord.1​  thanks for the exhaustive explanation.

Jan