2025-03-20 3:07 AM - edited 2025-03-20 3:10 AM
Good Morning,
I am working on the Secure Boot using STM32U5 with this repository : https://github.com/STMicroelectronics/STM32CubeU5/tree/main/Projects/B-U585I-IOT02A/Applications/SBSFU
I am trying to add a kind of "Dev. Mode" which authorise the boot even if the Application's flash is corrupted.
Are there any restriction from the SBSFU_Boot code or ROM code that prevents this feature ?
Moreover, do you have any links to the SBSFU_Boot.bin sources, especially the main.c or this part is private and can't be shared ?
Best Regards,
Loïc
Solved! Go to Solution.
2025-03-20 6:46 AM
Hello @lotou ,
You have access the the whole source code.
You can find the main in bl2_main.c located in mcuboot in Middlewares
There is no restriction, just a matter of changing the code to allow such behaviour
Best regards
Jocelyn
2025-03-20 6:46 AM
Hello @lotou ,
You have access the the whole source code.
You can find the main in bl2_main.c located in mcuboot in Middlewares
There is no restriction, just a matter of changing the code to allow such behaviour
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.