2021-12-16 12:39 AM
Hello,
I have here two Nucleos with an H743 on it. If it is rev Y, it is the "old" 144pin Nucleo board with the break-off ST-link board on top. For this there is a schematics in appendix A of the user manual. But if it is rev V, it is NUCLEO-H743ZI2 , note the 2 at the end, with no break-off possibility and a different user manual. And this manual has no schematics included. A trouble start as I start my project. While the manual says PC9 = MCO2 is on CN8 pin4 and CN12 pin1, I see a signal only on CN8 pin4. No way to check what's going on without schematics.
Please ST folks can you provide this somewhere.
Thanks a lot
Martin
Solved! Go to Solution.
2021-12-16 03:18 AM
Hello,
MB1137 schematics (NUCLEO-H743ZI) with ST-Link V2 : https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip
MB1364 schematics (NUCLEO-H743ZI2) with ST-Link V3 : https://www.st.com/resource/en/schematic_pack/mb1364-h743zi-c01_schematic.pdf
These links are available at the bottom of the CAD resources page:
https://www.st.com/en/evaluation-tools/nucleo-h743zi.html#cad-resources
2021-12-16 01:52 AM
Could you share me "which user manual you rely on?"
2021-12-16 01:59 AM
Hi Sco,
yes, sure, here are the manuals I use:
For the "old" 144pin Nucleo I have UM1974, page footer says DocID028599 Rev 7 December 2017
For the NUCLEO-H743ZI2 I have UM2407, page footer says UM2407 Rev 2, June 2020, which I downloaded just yesterday. This is the one I desire schematics for.
I hope you can help.
Martin
2021-12-16 03:18 AM
Hello,
MB1137 schematics (NUCLEO-H743ZI) with ST-Link V2 : https://www.st.com/resource/en/schematic_pack/nucleo_144pins_sch.zip
MB1364 schematics (NUCLEO-H743ZI2) with ST-Link V3 : https://www.st.com/resource/en/schematic_pack/mb1364-h743zi-c01_schematic.pdf
These links are available at the bottom of the CAD resources page:
https://www.st.com/en/evaluation-tools/nucleo-h743zi.html#cad-resources
2021-12-16 04:09 AM
Hi Mike,
thanks for this quick and complete answer - both thumbs up
Martin
2024-01-15 12:34 AM
Hello,
I bought one Nucleo-H743ZI2 board and found the two capacitors (C71 and C72) for X2 32.768KHz are not installed. May I know if I need to install them with 5.1pF if I want to use the X2? I went through the manual "UM2407 User manual for STM32H7 Nucleo-144 boards (MB1364)". But it seems not mention the two capacitors for the LSE clock. Thank you.
2024-01-15 06:07 AM
Hello @Jiaming and welcome to the community.
This thread is already closed and I suggest you to open a new one.
Thank you for your understanding.