2024-02-26 4:16 AM
2024-02-26 8:33 AM - edited 2024-02-28 8:06 AM
Hello,
FMC as Flexible Memory Controller and it manages parallel signals. It's used to connect external parallel devices like memories, LCDs etc. The interface has three types of signals: Data, Address and Control.
The following is an example of a connection of an SRAM and a NOR flash to STM32L476 device (STM32L476G-EVAL board).
So no relation with other protocols or comm interfaces such as SPI or UART ..
2024-02-26 6:00 AM
FMC is a peripheral to connect parallel memories.
So no, no SPI (which is a serial protocol).
JW
2024-02-26 8:33 AM - edited 2024-02-28 8:06 AM
Hello,
FMC as Flexible Memory Controller and it manages parallel signals. It's used to connect external parallel devices like memories, LCDs etc. The interface has three types of signals: Data, Address and Control.
The following is an example of a connection of an SRAM and a NOR flash to STM32L476 device (STM32L476G-EVAL board).
So no relation with other protocols or comm interfaces such as SPI or UART ..