Skip to main content
Associate
April 1, 2025
Solved

STM32WL33 modulation support for GMSK

  • April 1, 2025
  • 1 reply
  • 457 views

Hi,

The specifications mention multi-protocol support for 4-(G)FSK, 2-(G)FSK, (G)MSK, DBPSK, DSSS, and ASK. However, the reference manual does not explicitly mention GMSK.

Can the device demodulate GMSK directly through register settings, or is it only possible via raw IQ data and external software processing?

Best Regards

Arne

This topic has been closed for replies.
Best answer by STTwo-32

Hello @bobbe 

You can use simple 2GFSK modulation, with the difference that you need to select a modulation index of 0.5. Therefore, you should set the proper data rate and frequency deviation. 

Best Regards.

STTwo-32

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
April 2, 2025

Hello @bobbe 

You can use simple 2GFSK modulation, with the difference that you need to select a modulation index of 0.5. Therefore, you should set the proper data rate and frequency deviation. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.