2025-04-01 5:34 AM
Hi,
I am trying to interface Stm32h745 controller with a 240x320 TFT LCD over FMC. Interesting thing is, when I manually control lcd control and data pins(Set them as GPIO_OUTPUT_PP), Lcd works, but when I switched to FMC it does not. Tried lots of timing configuration but it did not help.
Here is the init for FMC
.Instance = FMC_NORSRAM_DEVICE;
.Extended = FMC_NORSRAM_EXTENDED_DEVICE;
.Init.NSBank = FMC_NORSRAM_BANK1;
.Init.DataAddressMux = FMC_DATA_ADDRESS_MUX_DISABLE;
.Init.MemoryType = FMC_MEMORY_TYPE_SRAM;
.Init.MemoryDataWidth = FMC_NORSRAM_MEM_BUS_WIDTH_8;
.Init.BurstAccessMode = FMC_BURST_ACCESS_MODE_DISABLE;
.Init.WaitSignalPolarity = FMC_WAIT_SIGNAL_POLARITY_LOW;
.Init.WaitSignalActive = FMC_WAIT_TIMING_BEFORE_WS;
.Init.WriteOperation = FMC_WRITE_OPERATION_ENABLE;
.Init.WaitSignal = FMC_WAIT_SIGNAL_DISABLE;
.Init.ExtendedMode = FMC_EXTENDED_MODE_DISABLE;
.Init.AsynchronousWait = FMC_ASYNCHRONOUS_WAIT_DISABLE;
.Init.WriteBurst = FMC_WRITE_BURST_DISABLE;
.Init.ContinuousClock = FMC_CONTINUOUS_CLOCK_SYNC_ONLY;
.Init.WriteFifo = FMC_WRITE_FIFO_DISABLE;
instance->deviceHandleAsRam.Init.PageSize = FMC_PAGE_SIZE_NONE;
FMC_NORSRAM_TimingTypeDef Timing = {0};
Timing.AddressSetupTime = 15; // 1 cycle = 16.67 ns
Timing.AddressHoldTime = 15; // 1 cycle hold time
Timing.DataSetupTime = 255; // 4 cycles ≈ 66.7 ns
Timing.BusTurnAroundDuration = 15;
Timing.CLKDivision = 16; // Unused in SRAM mode
Timing.DataLatency = 17; // Not used in mode A
Timing.AccessMode = FMC_ACCESS_MODE_A;
instance->deviceTiming = Timing;Tried FMC peripheral clk from 240 Mhz down to 15Mhz
LCD command/data selection connected to A0, and I am bank swapping from0x60000000 to 0xC0000000
#define LCD_BASE_ADDRESS ((uint32_t)0xC0000000)
#define Lcd_CmdWrite(cmd) *((__IO uint8_t*)LCD_BASE_ADDRESS) = cmd
#define Lcd_DataWrite(data) *((__IO uint8_t*)((LCD_BASE_ADDRESS) + (1 << (0 + 1)))) = data Here is the Logic Analyzer screen for 160Mhz Fmc Clock for the sequence below
And here is the same saquence output with manual GPIO Control
Thanks for any help
Solved! Go to Solution.
2025-05-13 3:59 AM
Hi Dor_Rh,
Thanks for the information. I already fixed the problem.
Best regards
Baycan
2025-05-13 3:51 AM
Hello @baycanakcay,
You might find this post helpful: Sending Data to TFT LCD via FMC Fails. It may assist you in your application by providing insights and solutions.
I hope this information is helpful. If it resolves your query, please mark this topic as the solution to assist others in finding the answer more quickly. Thank you for your contribution.
Best regards,
Dor_RH
2025-05-13 3:59 AM
Hi Dor_Rh,
Thanks for the information. I already fixed the problem.
Best regards
Baycan
2025-05-13 7:29 AM
Hello @baycanakcay,
Thank you for informing us about the resolution of the issue.
Could you share the solution or steps you took to resolve the problem?
This information could benefit other customers who may face similar challenges.
We appreciate your cooperation.
Best regards,
Dor_RH