2018-11-02 1:55 PM
In the STM32H743 errata sheet (ES0392 revision 4), section 2.3.1 “Conversion overlap may impact the ADC accuracy�? leaves me with three questions:
2018-11-02 5:45 PM
Great questions, hope to get some comments from ST.
I have experimented with overlapped (or better say purposely synchronized measurements) and do not see any deterioration. I have used 2x ADCs triggered by a timer simultaneously + third ADC running asynchronously - but still is expected to coincide sometimes + DAC -which is too supposed to cause issues.
But... the noise in my system is 8mV p-p at 3.3V supply. I do not see the ADC measuring worse noise than this. This noise level would mean ~ 150 LSBs at 16 bits that I use - so I guess my application is not very demanding.
One thing I found out, which was totally unexpected - PLL clock configurations may affect ADC results. No matter if one or more ADC is converting. I was getting random offsets on the channels, which kept changing with every reset around 8-16 mV up/down. It is channel dependent problem - some channels did not show any issues, while others showed random offsets. Resolved it by configuring PLL1 and PLL3 to be divisible on one another - took me weeks to find out... So the MCU definitely has issues. Hope they resolved it in rev X.
2018-11-02 5:53 PM
Interesting! Do you mean just the VCO frequencies, or did you have to modify the divider outputs as well? And I assume that you were using PLL3R as the ADC source in this case, since you say that it was PLL3 that affected you?
2018-11-03 7:35 AM
Yes, I am using PLL3R as ADC source. What worked for me was - setting VCOs identical for PLL1 and 3, then the final dividers P/Q/R are different, but I take care all 6 of them to have a common denominator - i.e. setting one to 32 and the other to 16 is OK, but 32 and 5 is not.
Not saying that this is the only way to make it work, but it resolved the random offset issues for me.
2019-08-22 4:38 PM
Hi Dan, did you trigger ADC by timer? Could your sampling phase noise be a result of ADC attempt to synchronize two clock sources (ADC and TIM)?