2018-10-11 2:49 PM
DS12110 Rev 5, notes for Figure 40. says it should be in Table 85 but it isn't. Rain and Cadc are in the Table 85.
2018-11-06 8:02 AM
Hello all,
Would also like to know the answer to this one.
Anyone any idea??
Regards,
2019-04-16 1:50 PM
I suspect it may differ for fast versus slow channels. I would also like to know.
2019-04-17 1:27 PM
I got a reply from ST in a support ticket. Their recommendation is to use table 185 in the datasheet (it’s in the revision V section, but the rep said it applies to revision Y as well).
2019-04-18 10:24 AM
The Rev 6 datasheet still calls out Radc in two places and says look for it in two tables. This note should be removed if Radc isn't going to be provided.