2020-05-13 12:13 AM
Hi all.
i using the ADC in STM32L412 MCU .
according to the DS , the current consumption of the ADC in Range 2 is 0.2uA/MHz for independent clock domain and 1.8uA/MHz for clock domain...
what is the "independent clock domain"
according to the DS , the ADC can run only at SYSCLK ( Figure 4. Clock tree )
2020-05-13 01:29 AM
I'd say, a copy/paste artefact from other 'L4 datasheets.
It decreases the credibility of the given value, though.
@Amel NASRI , can you please have a look at this?
Thanks,
JW
2020-05-13 01:32 AM
Btw.
which is probably bogus, too.
JW
2020-05-14 08:36 AM
Hi @Ach.1 & @Community member ,
I am checking these inconsistencies internally, will come back to you on this regard.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-05-16 09:17 PM
thanks @Amel NASRI & @Community member .
can you kindly also answer my other Q "STM32L4 ADC power consumption VS ADC FREQ"
that i didn't got no comment.
thanks.
2020-05-16 11:20 PM