2025-01-08 2:25 AM - last edited on 2025-01-08 3:10 AM by Andrew Neil
Originally a reply here: https://community.st.com/t5/stm32-mcus-products/using-swd-pins-to-flash-code/td-p/759046
Split to a new thread as this is a new question.
Thank you for the solution. However, I have another doubt here. While referring to: STM32H5 MCU hardware development. i came across-
Here it says for DFU (device firmware upgrade) for STM32H503 series is supported by PA11/ PA12. So does this mean that both SWDIO, SWCLK and the port PA11/PA12 can be used for the firmware update?
2025-01-08 3:11 AM
Please mark the solution in the other thread.
@bhoomika_patil wrote:does this mean that both SWDIO, SWCLK and the port PA11/PA12 can be used for the firmware update?
Yes - and all the other options.
But only SWD provides debug.
And you will have to provide additional hardware for USB ...
2025-01-08 3:43 AM - last edited on 2025-01-08 3:55 AM by Andrew Neil
duplicate - merged
Thank you for the explanation. However, while referring to STM32H5 MCU hardware development: i came across-
The table says that DFU (device firmware update) can be done using PA11/ PA12 for STMH503 series, so does this indicate that both SWDIO, SWCLK and PA11/PA12 can be used for software update?
2025-01-08 4:56 AM
But I have configured all other pins in my design and only left alone with SWDIO and SWCLK. So should it be a problem if I want update the firmware using these two pins?
2025-01-08 5:03 AM - edited 2025-01-08 5:04 AM
You marked the wrong post in the other thread - you need to mark which ever one you think actually provided the solution to your problem!
@bhoomika_patil wrote:But I have configured all other pins in my design
Obviously, if you want to use them for USB then you can't use them for anything else!