Using Break Functionality as interrupt in stm32f4
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-09 1:25 AM
For PWM channels to be disabled during a trip instant we use the break input circuit and the function worked well in the Nucleo board. But while using the same in the real circuit having half-bridge, cross conduction occurs every time the break input gets active.
we observed that the complementary waveform degrades to zero instead of immediately being pulled down to zero
- Is there any option to use the break as an interrupt?
- Is there any other option to force the output and its complementary channel to zero while using the break functionality?
Solved! Go to Solution.
- Labels:
-
STM32F4 Series
-
TIM
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-09 5:00 AM
- Yes, see TIMx_DIER.BIE, and the related interrupts (TIM1_BRK_TIM9, TIM8_BRK_TIM12 in case of STM32F4xx covered by RM0090).
- Yes, that's the purpose of TIMx_BDTR.OSSI bit (and related bits like TIMx_CR2.OISx/OISxN bits), see Output control bits for complementary OCx and OCxN channels with break feature table.
Read the Advanced Timers chapter in RM.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-09 4:19 AM
How did you configure the gate inputs on the bridge? If the STM32 PWM outputs go to tri-state (analog) mode do you have a pull-down to shut off the high side and a pull-up to short the motor windings to ground side? If you see shoot-through, how is that both high sides are enabled since only one should be active when the shutdown occurs?
Jack Peacock
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-09 5:00 AM
- Yes, see TIMx_DIER.BIE, and the related interrupts (TIM1_BRK_TIM9, TIM8_BRK_TIM12 in case of STM32F4xx covered by RM0090).
- Yes, that's the purpose of TIMx_BDTR.OSSI bit (and related bits like TIMx_CR2.OISx/OISxN bits), see Output control bits for complementary OCx and OCxN channels with break feature table.
Read the Advanced Timers chapter in RM.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-12 2:38 AM
Hi @Jeflet ,
Besides to the reference manual already mentioned by @Community member , look to the application note AN4277: Using STM32 device PWM shut-down features for motor control and digital power conversion.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.