User Activity

While testing the exception traps routines I ran into an odd problem with the SRAM2 parity check on an STM32L496. As part of a unit test I force a usage error by attempting to read from 0x3000 0000, an invalid address. The usage vector is called co...
I configured the SPI2 port for bidirectional (BIDIMODE = 1) and rx (BIDIOE = 0), then enabled the port (SPE = 1). According to the RM the enable should immediately start sending clock pulses out the SCK pin and read data on the MOSI pin, since it is...
As of Monday 2019-01-14 my Atollic 9.1.0 IDE has stopped working with Microsoft Devops as the cloud repo. I use the Microsoft TEE Eclipse plugin from Github, latest version. It's worked very well for the last three months, uploads, downloads, etc. ...
Kudos from