2019-08-28 08:31 AM
Hello, I'm working with F746ZG Nucleo board with fw package STM32Cube FW_F7 V1.15.0. I seem that the included user manual UM1905 is not updated: C functions related to the CAN described in the document don't correspond to the function interfaces defined in the driver source code. Where can I find an updated version?
2019-09-04 02:33 AM
Hi @LPane ,
UM1905 wasn't updated since February 2017, I submitted an internal request to align it with last firmware changes.
Meanwhile, you can refer to:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-09-04 03:24 AM
Hello,
Thanks for the answer.
Please, could you tell me which is the release note you refer, that is the name of the document and also where I can find the CHM files?
Luca
2019-09-04 04:12 AM
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.