2022-08-22 2:36 AM
Hi all,
I have a question regarding the control of the UART interrupt on the STM32F4.
First let me describe the application:
int main(void)
{
SystemInit();
//Stream out Data via Uart via DMA
HAL_UART_Transmit_DMA(&huart2, (uint8_t *)UARTMessage_out, MSGLENGTH);
//Enable UART Rx interrupt in order to receive messages over Terminal
HAL_UART_Receive_IT(&huart2, dataRx, 1);
/* Infinite loop */
while (1)
{
ADCRead();
Computations();
DACWrite();
//In this section the transmit Interrupt is allowed to fire
HAL_NVIC_EnableIRQ(DMA1_Stream6_IRQn);
if(DMAReady == 1)
{
GenerateUARTMsg();
DMAReady=0;
UART_DMA_Transmit()
}
//here the UART transmit interrupt again disabled
HAL_NVIC_DisableIRQ(DMA1_Stream6_IRQn);
}
}
//Callback when MCUout/PCin Message is done
//Here the time between two Messages is measured
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart)
{
timer = __HAL_TIM_GetCounter(&htim2);
__HAL_TIM_DISABLE(&htim2);
__HAL_TIM_SetCounter(&htim2,0); //reset counter back to zero
DMAReady = 0; /
__HAL_TIM_ENABLE(&htim2);
}
void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)
{
ProcessInput();
HAL_UART_Receive_IT(&huart2, dataRx, 1);
}
Somehow the disable of the DMA interrupt (HAL_NVIC_DisableIRQ(DMA1_Stream6_IRQn);) does not work.
When I disable the whole uart interrupt via HAL_NVIC_EnableIRQ(USART2_IRQn) it works. But then also the receive interrupt is disabled. But the receive interrupt is allowed to fire all the time.
Background:
Uart transmit interrupt is for monitoring the adc values. This process shall not interrupt the ADC->Compute->DAC routine.
UART receive changes compute parameters. For this, the Data cycle is allowed to be interrupted.
Thanks in advance for your help!
Solved! Go to Solution.
2022-08-23 1:49 AM
Ok I found the solution for this problem.
I use the macros:
__HAL_UART_ENABLE_IT(&huart2,UART_IT_TC);
and the
__HAL_UART_DISABLE_IT(&huart2,UART_IT_TC);
Here the arg UART_IT_TC: Transmission complete interrupt.
It works in this context. I dont know however if this is the best solution.
2022-08-22 2:38 AM
Ahh stupid.
Of course in the transmit callback the flag must be
DMAReady=1;
Somehow I cannot edit the first post?
2022-08-23 1:49 AM
Ok I found the solution for this problem.
I use the macros:
__HAL_UART_ENABLE_IT(&huart2,UART_IT_TC);
and the
__HAL_UART_DISABLE_IT(&huart2,UART_IT_TC);
Here the arg UART_IT_TC: Transmission complete interrupt.
It works in this context. I dont know however if this is the best solution.