Skip to main content
YAtta.1
Associate
March 22, 2021
Question

copying a dual-core project

  • March 22, 2021
  • 1 reply
  • 545 views

I have problem with duplicating an existing dual-core project in STM32CubeIDE. in single core project it was just sufficient to copy and paste a project to save it with another name. but for dual core project this doesnot work. hoe can we duplicate an existing dual-core project in STM32CubeIDE?

    This topic has been closed for replies.

    1 reply

    'SMike
    Associate III
    August 22, 2022

    This is also an issue when storing the project in git and cloning to another workspace. This is a very basic activity that should be supported.