2023-08-23 1:35 AM
Hello,
I am trying to use UART HAL with the stm32-f030r8 connected to the PC through a USB-TTL module.
The configuration is given below :
- The F030R8 has JP1 OFF, JP6 ON, JP5 on E5V.
- The USB-TTL is :
- The code is :
/* Includes ------------------------------------------------------------------*/
#include "main.h"
uint8_t test[] = "hello";
UART_HandleTypeDef huart2;
int main(void)
{
HAL_Init();
SystemClock_Config();
__USART2_CLK_ENABLE();
__GPIOA_CLK_ENABLE();
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.Pin = GPIO_PIN_2;
GPIO_InitStructure.Mode = GPIO_MODE_AF_PP;
GPIO_InitStructure.Alternate = GPIO_AF1_USART2;
GPIO_InitStructure.Speed = GPIO_SPEED_HIGH;
GPIO_InitStructure.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.Pin = GPIO_PIN_3;
GPIO_InitStructure.Mode = GPIO_MODE_AF_OD;
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure);
huart2.Instance = USART2;
huart2.Init.BaudRate = 9600;
huart2.Init.WordLength = UART_WORDLENGTH_8B;
huart2.Init.Parity = UART_PARITY_NONE ;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.StopBits = UART_STOPBITS_1;
while (1){
HAL_UART_Transmit(&huart2,test,sizeof(test),HAL_MAX_DELAY);
HAL_Delay(1000);
}
}
Then, the putty configuration is 9600 baud, 8 data bits, 1 stop bits, no parity; no flow control.
But I can't see anything in the terminal...
Would you please have suggestions ?
Thanks for your help ! :)
2023-08-23 1:59 AM
t is not clear from the schematic if the Rx and Tx labels are for the module or for connecting to an external UART. Maybe the signals are mixed up. But the second problem is the signal level. TTL is for 5V logic, but the MCU uses 3.3V logic. If the MCU pins are not 5V tolerant, the MCU can also be destroyed. I would recommend using a TTL-3.3V level converter.
2023-08-23 2:41 AM
The Rx and Tx labels are for the wire of the USB-TTL converter : Tx for the green one connected to PA2, Rx for the white one connected to PA3.
2023-08-23 3:28 AM
Hello @ONadr.1 ,
you can refer to the user manual UM1724 Rev 14 Table 11. ARDUINO® connectors on NUCLEO-F030R8, NUCLEO-F070RB, It is mentioned USART2_TX and USART2_RX are linked to PA2 and PA3 respectively. USART2 by default is used for STLINK module.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-23 3:34 AM
Hello @user-stm,
You may need to check the schematic of the board
As you can see, some changes are needed to work with USART2. Otherwise, you can simply try different USART instance.
Hope this helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-23 4:55 AM - edited 2023-08-23 5:07 AM
As a beginner not really familiar with it, would you please detail needed changes ? Thanks !
2023-08-23 5:33 AM
Hi again @user-stm,
you can disconnect SB13, SB14 and use CN3 to drive TX and RX pins of USART2.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-08-24 12:29 AM
Another question then :
As it is mentioned that "By default, the USART2 communication between the target STM32 and ST-LINK MCU is enabled", if we forget the USB-TTL module ie we have a unique wire (USB Type-A to Mini-B cable) between the PC and the stm32, do you know why is still have anything on putty ?
Configuration with JP1 OFF, JP6 ON and JP5 on U5V and the following code :
2023-08-24 12:34 AM
Remove the 5V wire between the dongle and the board. The dongle receives its power from USB.
2023-08-24 12:51 AM - edited 2023-08-24 1:02 AM
If you refer to my last post, there is only one cable (USB Type-A to Mini-B cable) between the PC and the stm32, no USB-TTL module and JP5 on U5V.
In the configuration presented in the first post, there is no USB Type-A to Mini-B cable, only one USB-TTL module (with 5v, GND, tx,rx wires) between the board and the PC, and JP5 on E5V.