cancel
Showing results for 
Search instead for 
Did you mean: 

Two ADC in dual REGULAR SIMULTENIOUS mode

Pooja321
Associate II

I am trying to run both ADC in dual REGULAR SIMULTENIOUS mode (ADC1 as master and ADC2 as salve) ADC Converted Result shall be stored in an Array Buffer using DMA transfer (single channel only), ADC conversion trigger shall not be software based (we are selecting Tigger Source as TIM1).

i am using STM32G474RE Board.

 

 

2 REPLIES 2
mƎALLEm
ST Employee

Hello,

What is the question/issue?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Hello ,

I have already been using Triple ADC (ADC1, ADC2, ADC3) in interleaved mode in STM32F407 in another project (It is running perfectly fine), whereas with G4-series same configuration not working as expected.