cancel
Showing results for 
Search instead for 
Did you mean: 

Trigger ADC1 scan using TIM1 CC1 on F410RB

massimiliano2399
Associate II
Posted on September 20, 2016 at 13:08

Hi,

I use STM32F410RB, and I need to trigger an ADC1 scan regular conversion every TIM1 CC1 event.

I am sure that TIM1 works, because I have an interrupt that is triggered every CC1 event.

I tried to configure ADC as follows:


ADC_ChannelConfTypeDef sConfig;


/* ADC Initialization */

AdcHandle.Instance = ADC1;


AdcHandle.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;

AdcHandle.Init.Resolution = ADC_RESOLUTION_12B;

AdcHandle.Init.ScanConvMode = ENABLE;

AdcHandle.Init.ContinuousConvMode = DISABLE;

AdcHandle.Init.DiscontinuousConvMode = DISABLE;

AdcHandle.Init.NbrOfDiscConversion = 0;

AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;

AdcHandle.Init.ExternalTrigConv = ADC_EXTERNALTRIGCONV_T1_CC1;

AdcHandle.Init.DataAlign = ADC_DATAALIGN_RIGHT;

AdcHandle.Init.NbrOfConversion = 2;

AdcHandle.Init.DMAContinuousRequests = DISABLE;

AdcHandle.Init.EOCSelection = ADC_EOC_SINGLE_CONV;


HAL_ADC_Init(&AdcHandle);


/* Configure ADC3 regular channel */

sConfig.Channel = ADC_CHANNEL_0;

sConfig.Rank = 1;

sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;

sConfig.Offset = 0;


HAL_ADC_ConfigChannel(&AdcHandle, &sConfig);


/* Configure ADC3 regular channel */

sConfig.Channel = ADC_CHANNEL_1;

sConfig.Rank = 2;

sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;

sConfig.Offset = 0;


HAL_ADC_ConfigChannel(&AdcHandle, &sConfig);


HAL_ADC_Start_IT(&AdcHandle);

But ADC no interrupt is triggered.

Which register, which bit are involved in the configuration?

best regards

Max

#adc #timer #stm32f410rb

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Posted on November 08, 2017 at 20:44

Experimenting may be fun, but the primary source of information is (ought to be) the RM/DS.

If only Cube and the RM/DS came from the same universe. Of course I refer to the RM/DS in attempting to understand what Cube has emitted. It's always an adventure (on the other hand, it's easier than trying to use MSP430 peripherals, but I digress).

So you wanted to use one of the PWM modes. I don't know how are they called in the Cube parlance.

That's what I thought. I tried 'Active on match' thinking that sounded like a reasonable suspect. Didn't work. Now I'm thinking perhaps I need to reverse engineer the documentation further to figure out what other output mode configuration is required. If only there was a relevant ST example - like, say, the test code they used to qualify this functionality in test. But I fantasize.

Toggle is fine too if it fits other purposes that timer may be used for.

Toggle rather annoys me; it's a hack. It works - and isn't the ISR-based workaround described elsewhere - but it's clearly a hack.

Perhaps I can spend another hour or two and figure out what ST's documentation is trying to tell me, or what it neglects to mention.

Cheers.

Posted on November 08, 2017 at 20:56

[STM32Cube_FW_F4_V1.15.0]\Drivers\STM32F4xx_HAL_Driver\Inc\stm32f4xx_hal_tim.h :

/** @defgroup TIM_Output_Compare_and_PWM_modes  TIM Output Compare and PWM modes

  * @{

  */

&sharpdefine TIM_OCMODE_TIMING                   0x00000000U

&sharpdefine TIM_OCMODE_ACTIVE                   (TIM_CCMR1_OC1M_0)

&sharpdefine TIM_OCMODE_INACTIVE                 (TIM_CCMR1_OC1M_1)

&sharpdefine TIM_OCMODE_TOGGLE                   (TIM_CCMR1_OC1M_0 | TIM_CCMR1_OC1M_1)

&sharpdefine TIM_OCMODE_PWM1                     (TIM_CCMR1_OC1M_1 | TIM_CCMR1_OC1M_2)

&sharpdefine TIM_OCMODE_PWM2                     (TIM_CCMR1_OC1M)

&sharpdefine TIM_OCMODE_FORCED_ACTIVE            (TIM_CCMR1_OC1M_0 | TIM_CCMR1_OC1M_2)

&sharpdefine TIM_OCMODE_FORCED_INACTIVE          (TIM_CCMR1_OC1M_2)

So you want TIM_OCMODE_PWM1 instead of TIM_OCMODE_TIMING .

This is the reason why I find 'libraries' superfluous. I wouldn't touch Cube with a stick. YMMV.

JW

Posted on November 08, 2017 at 21:08

So you want TIM_OCMODE_PWM1 instead of TIM_OCMODE_TIMING .

Thanks. Why is this different than TIM_OCMODE_ACTIVE in terms of triggering the ADC? I'd expect one TIM1-clock width pulse at OC1REF with TIM_OCMODE_ACTIVE as long as the CCR register value is inside the up-count range of TIM1.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.