cancel
Showing results for 
Search instead for 
Did you mean: 

To generate the SPI clock SCLK without data transfer

Jagath
Associate II

Hello,

I am using STM32F446RE controller to communicate with TLC2578 old ADC converter through SPI communication.

To initialize the ADC first CS should be LOW and 16 clock - SCLK cycles need to issued.

  1. How to start the SPI clock without data transfer.
  2. Will the SPI clock starts after pulling CS low.

Thank you

Jagath

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

How is this different from transmitting 0x0000 or 0xFFFF?

The hardware NSS handling is mostly unusable anyway, so you want to handle CS "manually" (as GPIO Output) anyway.

JW