2015-12-29 7:00 AM
Hi all,
I've downloaded the following simple code in my STM32F3DISCOVERY but I don't see anything. Should be a sistem clock config problem?In main.c:&sharpinclude ''stm32f30x.h'' /***************************************/ void RCC_Configuration(void){ /* Enable GPIO clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE); /* Enable TIM3/4 clock */ RCC_APB1PeriphClockCmd( RCC_APB1Periph_TIM4, ENABLE);} /************************/ void GPIO_Configuration(void){ GPIO_InitTypeDef GPIO_InitStructure; GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_10); // TIM4_CH1 GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_10); // TIM4_CH2 GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11 | GPIO_Pin_12; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure);} /************************************/ void TIM_Configuration(void){ TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_OCInitTypeDef TIM_OCInitStructure; TIM_TimeBaseStructure.TIM_Prescaler = 72 - 1; // 72 to 1 MHz TIM_TimeBaseStructure.TIM_Period = 10 - 1; // 1 MHz to 100 KHz TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM4, &TIM_TimeBaseStructure); TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable; TIM_OCInitStructure.TIM_Pulse = 10 / 4; // 25% TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High; TIM_OC1Init(TIM4, &TIM_OCInitStructure); TIM_OC2Init(TIM4, &TIM_OCInitStructure); TIM_Cmd(TIM4, ENABLE); } /**************************************/ int main(void){ RCC_Configuration(); GPIO_Configuration(); TIM_Configuration(); while(1); // Don't want to exit}and I've this in system_stm32f30x.c :/* Select the PLL clock source *///&sharpdefine PLL_SOURCE_HSI // HSI (~8MHz) used to clock the PLL, and the PLL is used as system clock source//&sharpdefine PLL_SOURCE_HSE // HSE (8MHz) used to clock the PLL, and the PLL is used as system clock source&sharpdefine PLL_SOURCE_HSE_BYPASS // HSE bypassed with an external clock (8MHz, coming from ST-Link) used to clock Can you help me?Thanks in advantage. #pwm #stm32-mco-clock-output2015-01-02 9:40 AM
Hi Clive and Happy New Year.
Thank you very much, I'm investigating and I'll came back with the explanation.2015-12-29 12:19 PM
Should be a system clock config problem?
Ok, and that relates to the issue how? The system starts with a different clock, you're not saying the PWM is slower, but rather that it doesn't exist. Have you been able to step through the code, and check the pins with a scope? Aren't PA11/12 committed to USB on the F3-DISCO? Check it gets to main() and doesn't get stuck somewhere in SystemInit() If you want to check internal clocks, output via MCO (PA8)
2015-12-30 12:19 AM
Thank you Clive,
your comments are really helpful and appreciate. I've checked the pins with the scope. I've a question: what does mean ''Aren't PA11/12 committed to USB on the F3-DISCO'' ?I'd like to check the MCO via PA8, as you suggest, but I have a doubt how to set the TIM_OCInitStructure.TIM_OCMode and the TIM_TimeBaseStructure, can you help me?2015-12-30 6:21 AM
Check the Manual/Schematic, aren't the pins you are talking about connected to the USER USB? Does that conflict with your use? Do you need to change solder bridges to get to pins?
void OutputHSE2MCO(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* Output HSE clock on MCO1 pin(PA8) ****************************************/
/* Enable the GPIOA peripheral */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA, ENABLE);
/* Configure MCO1 pin(PA8) in alternate function */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* HSE clock selected to output on MCO1 pin(PA8)*/
RCC_MCOConfig(RCC_MCOSource_HSE);
}
2016-01-04 10:36 AM
It was a problem of broken code in the flash. I've reset with BOOT pin at 3V and now it works.
A previuos discussion is