2024-09-23 8:35 PM - last edited on 2024-09-24 6:21 AM by TDK
When I sent an SPI commnad to get the status from an SPI NAND, an extra clock was sent by the STM32F4.
I chedked the waveform with a logic analyzer.
An 8-bit command was sent to D0.
An 8-bit address was sent to D0.
There were 9 clocks sent by the controller to get data from D1.
I expected only 8 clocks.
The behavior of the SPI slave or SPI NAND was correct. It replied the 8-bit data normally.
The board I used is NUCLEO-F412ZG.
The tool I use is STM32CubeIDE.
The code I worte was given below.
/////////////////////
QSPI_CommandTypeDef sCommand;
QSPI_AutoPollingTypeDef sConfig;
/* Configure automatic polling mode to wait for memory ready ------ */
sCommand.InstructionMode = QSPI_INSTRUCTION_1_LINE;
sCommand.Instruction = READ_STATUS_REG_CMD;
sCommand.AddressMode = QSPI_ADDRESS_1_LINE;
sCommand.AddressSize= QSPI_ADDRESS_8_BITS;
sCommand.Address = addr;
sCommand.AlternateByteMode = QSPI_ALTERNATE_BYTES_NONE;
sCommand.DataMode = QSPI_DATA_1_LINE;
sCommand.DummyCycles = 0;
sCommand.DdrMode = QSPI_DDR_MODE_DISABLE;
sCommand.DdrHoldHalfCycle = QSPI_DDR_HHC_ANALOG_DELAY;
sCommand.SIOOMode = QSPI_SIOO_INST_EVERY_CMD;
sCommand.NbData = 1;
//check the status automatically
sConfig.Match = match;
sConfig.Mask = mask;
sConfig.MatchMode = QSPI_MATCH_MODE_AND;
sConfig.StatusBytesSize = 1;
sConfig.Interval = 0x10;
sConfig.AutomaticStop = QSPI_AUTOMATIC_STOP_ENABLE;
if (HAL_QSPI_AutoPolling(&hqspi, &sCommand, &sConfig, HAL_QPSI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
{
return HAL_ERROR;
}
return HAL_OK;
/////////////////////
2024-09-23 11:06 PM
This looks like a classic case of the wrong CPOL and/ or CPHA setting...
Kind regards
Pedro
2024-09-24 6:26 AM
I've changed your title to reflect that you're asking about QUADSPI, not SPI.
Not sure on the question. If you increase dummy cycles to 1, does the number of bits increase by 1 (to 2 extra)?
Might be something with auto polling. Does the same happen with HAL_QSPI_Command + HAL_QSPI_Receive?
2024-09-24 6:37 AM
Please see the posting tips for how to properly post source code:
2024-09-24 6:58 AM
Show initialization code.
Clear auto/local variables in a function as they can contain random junk.