2024-06-01 01:56 AM - edited 2024-06-01 04:04 AM
Hello, I have a question regarding the subject.
Thank you always for your great answers. They have been very helpful 😀
[Reproduction Steps]
1. In CubeProgrammer, select the following External Loader:
MT25TL01G_STM32H750B-DISCO.stldr
> C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\ExternalLoader
> The Page Size is 0x1000, but according to the Datasheet, I believe the correct value should be 0x100.
2. In the Erasing & Programming menu, select Full chip erase.
3. In the Erasing & Programming menu, select a 4-byte binary file and start programming.
Binary content: 0xA1B2C3D4 Start address: 0x98000000
> The STM32H750B has 1Gbit, so the range should be 0x90000000~0x97FFFFFF.
> Even if you write to 0x98000000, Download & Verify succeeds. (??? should not be accessible)
4. In the Memory & File editing menu, specify the address 0x97FFFFF0 and read.
> Data is written at the 0x98000000 location.
5. In the Erasing & Programming menu, select a 4-byte binary file and start programming.
Binary content: 0xF5E6D7C8 Start address: 0x98000000
> This time, "Error: Download verification failed" occurs.
6. In the Memory & File editing menu, specify the address 0x97FFFFF0 and read.
> The data at the 0x98000000 location is suspicious.
7. If you try to write a 4-byte binary to addresses like 0x98000004/0x98000008, it fails.
> This is the correct behavior.
[Questions]
These questions related to the `MT25TL01G_STM32H750B-DISCO.stldr`.
Q1. Is the Page Size of 0x1000 incorrectly specified?
Q2. Why is it possible to write data to 0x98000000?
Q3. Although there is no source code, if I check the assembly, `hqspi.Init.FlashSize` is set to 27.
Since 27 corresponds to 2Gbit Flash size, it should be 26 for the H750B.
Is there a reason for set 27?
By the way, when I create the External Loader from scratch and set FlashSize to 26,
there was a problem where the last 2 bytes of the 0x97FFFFFE~0x97FFFFFF range referenced incorrect values in CubeProgrammer and CubeIDE(debug) after entering Memory Mapped Mode.
So, was 27 set to avoid this issue for `MT25TL01G_STM32H750B-DISCO.stldr`?
Solved! Go to Solution.
2024-06-04 10:21 PM
I think this is related to following thread.
https://community.st.com/t5/stm32-mcus-products/h7-quadspi-weirdness/m-p/258686
Also, the errata sheet ES0392 mentions the same problem.
Which is a better approach?
2024-06-04 10:21 PM
I think this is related to following thread.
https://community.st.com/t5/stm32-mcus-products/h7-quadspi-weirdness/m-p/258686
Also, the errata sheet ES0392 mentions the same problem.
Which is a better approach?