2024-08-20 10:53 PM
When will support for the STM32U073 be added to the Arduino package? I just updated to 2.8.1, but still no support for the STM32U073. Just a Generic STM32U073KB is all I need. Of course, this means that appropriate code libraries for the U0 need to be in place, but I expect this has been done for the CUBE environment.
Thank you!
jim
2024-08-20 11:18 PM
Maybe https://www.stm32duino.com/ is a more appropriate place for this question.
JW
2024-08-21 01:01 AM - edited 2024-08-21 02:34 AM
2024-08-21 02:27 AM
@STTwo-32 wrote:The necessary support will be provided here (sic?).
Did you mean, "there" - ie, on the STM32duino GitHub ?
2024-08-21 02:34 AM
Sorry for the Typo 🙏, Yes, I mean there.
Thanks.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-21 02:41 AM
Purely out of interest, is STM32duino an official ST project?