cancel
Showing results for 
Search instead for 
Did you mean: 

Support for STM32U073 in Arduino

doctek
Associate II

When will support for the STM32U073 be added to the Arduino package? I just updated to 2.8.1, but still no support for the STM32U073. Just a Generic STM32U073KB is all I need. Of course, this means that appropriate code libraries for the U0 need to be in place, but I expect this has been done for the CUBE environment.

Thank you!

                  jim

6 REPLIES 6

Maybe https://www.stm32duino.com/  is a more appropriate place for this question.

JW

STTwo-32
ST Employee

Hello @doctek 

I suggest you follow this post. I think is yours. The necessary support will be provided there.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


@STTwo-32 wrote:

The necessary support will be provided here (sic?).


Did you mean, "there" - ie, on the STM32duino GitHub ?

Sorry for the Typo , Yes, I mean there.

Thanks.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Purely out of interest, is STM32duino an official ST project?

Hi @Andrew Neil 

STM32duino GitHub organization is a community project, it is not part of the official software ecosystem supported by ST. Nevertheless ST contributes to this community.

For question, support, ..., you could submit a topic on the stm32duino forum or open a discussion here.

If you have any issue, you could file an issue on one of the repository of the stm32duino GitHub organization.

BR

https://github.com/stm32duino