2024-03-11 01:51 AM
How to open the STSW-IO-LINK evaluation firmware in the STM32CubeMX development platform? STSW-IO-Link is downloaded and extracted. The *.ioc file seems to be missing in the STSW-IO-LINK firmware package!
Solved! Go to Solution.
2024-03-12 03:34 AM
1. STSW-IO-LINK firmware is developed using IAR.
2. take a look at this video.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-11 02:26 AM
Hello @Luna and welcome to the ST Community
The examples of this firmware are not developed starting from CubeMX configurations. So, there is not a .ioc file on the projects.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-11 06:29 PM
thanks for your information. if I want to change the firmware code and download it to MCU, do i need to start from 0 to create my own project and code? or do I have any other ways more easier?
2024-03-11 08:38 PM
Changes should be done directly on the code or by starting a new project.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-11 10:06 PM - edited 2024-03-11 10:29 PM
ok, here are 2 more questions.
1. may I know which develop environment used to develop STSW-IO-LINK firmware if it is not CubeMX?
2. the default firmware in STEVAL-IDP004V2 is STSW-IO-LINK or not?
thanks.
2024-03-12 03:34 AM
1. STSW-IO-LINK firmware is developed using IAR.
2. take a look at this video.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-12 03:46 AM
@Luna wrote:1. may I know which develop environment used to develop STSW-IO-LINK firmware if it is not CubeMX?
CubeMX just creates configuration code for the hardware - it doesn't affect the rest of the code that you develop...
2024-03-12 10:33 PM
thanks.
since I have flashed the MCU with other firmware version, where can I get the default firmware version when I bought?
2024-03-12 10:39 PM
if i will use CubeMX, I need to configure the .ioc by myself and use the code provided by ST, to make it co
2024-03-13 12:25 AM
Since Your original problem was solved. I suggest you close this post by choosing a best answer and open a new thread on the Interface and connectivity ICs for the new request to give it more visibility.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.