STM32U535VE / Pin configuration table / Excel or CSV-table
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-09 06:29 AM
Hello, is there any possibility to get the pin configuration table for the STM32U535VE in CSV or Excel format?
Thanks a lot !
Ricos
Solved! Go to Solution.
- Labels:
-
STM32U5 Series
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 03:22 AM
Hi @RicOs ,
I join @Andrew Neil with the idea to use STM32CubeMX.
From Pinout tab, STM32CubeMX allows to export the pinout to a csv file. You can select any STM32 part number then do the required export. This is explained in the UM1718:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-09 06:53 AM
Yes, it would be really useful if the pinout table, alternate function table, etc were made available in an easy machine-readable format - rather than just as text in the Datasheet & Ref Manual.
I'm sure I've requested this before.
One thing you can do is to create a project in CubeMX, and then use Project > Generate Report
Or the IBIS files will give you a start - with pin number & name; eg,
|************************************************************************
| stm32f0_440_lqfp32 IBIS Model
|************************************************************************
[IBIS ver] 4.2
[File name] stm32f0_440_lqfp32.ibs
[File Rev] 1.0
[Date] 15-5-2013
[Source] Data Created at STMicroelectronics
[Notes] File originated from ELDO simulations.
[Disclaimer] This information is for modeling purpose only and is
not guaranted. The information is subject to change without
notice.
[Copyright] Copyright 2015 STMicroelectronics Inc.
|
[Component] stm32f0_440_lqfp32
[Manufacturer] STMicroelectronics
[Package]
| variable typ min max
R_pkg 0.0 NA NA
L_pkg 0.0H NA NA
C_pkg 0.0F NA NA
|
[Pin] signal_name model_name R_pin L_pin C_pin
1 VDD POWER 0.03449 2.11E-09 6E-14
2 PF0 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
3 PF1 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
4 NRST ioreset_tc_v33 0.024645 1.09E-09 1E-14
5 VDDA POWER 0.024645 1.09E-09 1E-14
6 PA0 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
7 PA1 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
8 PA2 io8p_sudq_ft 0.03449 2.11E-09 6E-14
9 PA3 io8p_sudq_ft 0.03449 2.11E-09 6E-14
10 PA4 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
11 PA5 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
12 PA6 io8p_sudq_ft 0.024645 1.09E-09 1E-14
13 PA7 io8p_sudq_ft 0.024645 1.09E-09 1E-14
14 PB0 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
15 PB1 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
16 VSS GND 0.03449 2.11E-09 6E-14
17 VDD POWER 0.03449 2.11E-09 6E-14
18 PA8 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
19 PA9 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
20 PA10 io8p_sudq_ft 0.024645 1.09E-09 1E-14
21 PA11 io8p_sudq_ft 0.024645 1.09E-09 1E-14
22 PA12 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
23 PA13 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
24 PA14 io8p_sudq_ft 0.03449 2.11E-09 6E-14
25 PA15 io8p_sudq_ft 0.03449 2.11E-09 6E-14
26 PB3 io8p_sudq_ft 0.029020556 1.54333E-09 3.22222E-14
27 PB4 io8p_sudq_ft 0.025738889 1.20333E-09 1.55556E-14
28 PB5 io8p_sudq_ft 0.024645 1.09E-09 1E-14
29 PB6 io8p_sudq_i2cin_lv_ft 0.024645 1.09E-09 1E-14
30 PB7 io8p_sudq_i2cin_lv_ft 0.025738889 1.20333E-09 1.55556E-14
31 BOOT0 vpp_test_hv 0.029020556 1.54333E-09 3.22222E-14
32 VSS GND 0.03449 2.11E-09 6E-14
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-09 07:52 AM
Thanks Andrew. In my work I only define the functions of the pins, so such a table is suitable to provide results. I hope ST can provide a table as useful as other providers already do.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-10 01:55 AM
@RicOs wrote:a table as useful as other providers already do.
Out of interest, which other providers have you found which do that?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 03:22 AM
Hi @RicOs ,
I join @Andrew Neil with the idea to use STM32CubeMX.
From Pinout tab, STM32CubeMX allows to export the pinout to a csv file. You can select any STM32 part number then do the required export. This is explained in the UM1718:
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 03:39 AM
Does/can the CubeMX export actually give a full listing of all a part's chips?
It seems to only list the ones that are actually used by a project, as used by that project?
So not a complete listing of all the pins with all the AF options and all the Additional Function options?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 03:51 AM
@Andrew Neil wrote:So not a complete listing of all the pins with all the AF options and all the Additional Function options?
@Amel NASRI something like this - see attached
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 04:39 AM
I tested it for STM32C0 (WLCSP12 package) and got the following:
Do you see missing information?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 05:22 AM
Ah, right - I was looking at the Project Report rather than the pinout export.
The Project Report does only list used pins & AFs.
The pinout export is missing the "Additional" functions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-01-15 05:50 AM
Just to complete @Amel NASRI 's answer, as sometime the most difficult is to find the function in the tool, below the picture to find the mention menu in STM32CubeMX.