2020-04-26 09:51 AM
RM0351 and RM0392 (and maybe others, haven't checked them all) contain this in the System clock (SYSCLK) selection section
Status bits in the Internal clock sources calibration register (RCC_ICSCR) indicate which clock(s) is (are) ready and which clock is currently used as a system clock.
However the various clock ready and system clock switch status bits are actually located in RCC->CR and RCC->CFGR.
2020-04-27 07:22 AM
Hello,
I raised this internally for update.
Thank you for your contribution.
Best Regards,
Imen
2020-04-27 12:14 PM
Hi @Imen DAHMEN ,
I've seen the same sentence also in RM0440 and RM0444, so this propagates across families.
Jan