cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L452 LSE not starting

SLevi.1
Senior

I have an STM32L452 rigged to use an external clock so we can keep the RTC running. Schematic attached.LSE_schem.png

X2 is a clock from SiTime, programmed to be 32.768kHz. C36 is a supercap acting as battery backup. I used STMCube to generate the startup code to feed into HAL_RCC_OscConfig. When I debug into this function, the LSE never becomes ready (RCC_BDCR_LSERDY bit always zero), and so the code returns HAL_TIMEOUT.

Do I have the correct circuit? Have I set the clock config correctly? It's the same if I run on a Nucleo board.

/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 2;
RCC_OscInitStruct.PLL.PLLN = 36;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV4;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV4;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}

1 ACCEPTED SOLUTION

Accepted Solutions

Turns out that the wrong clock chip had been fitted - they'd used the low-power variant, so the swing on the clock signal was not sufficient for the processor to detect.

View solution in original post

18 REPLIES 18
gbm
Principal

Did you select BYPASS option in LSE configuration? I guess not -> check and correct.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
AScha.3
Super User

where is the vbat power coming from ?? CPHxx is a big cap - and empty. needs some diode or so from vdd -> cap, to charge it. otherwise the 32khz osc never gets power.

If you feel a post has answered your question, please click "Accept as Solution".

I've tried LSE ON and LSE BYPASS; both give the same result. 

My colleagure assures me he can see the 32768Hz clock on a scope. I use VBAT output to pwoer the supercap thus:

// Enable VBat output, which allows supercap to charge and external 32.678 clock to run
// thereby keeping RTC correct in 12v power loss
//
// Bit 9 VBRS: VBAT battery charging resistor selection
// 0: Charge VBAT through a 5 kOhms resistor
// 1: Charge VBAT through a 1.5 kOhms resistor
// Bit 8 VBE: VBAT battery charging enable
// 0: VBAT battery charging disable
// 1: VBAT battery charging enable
PWR->CR4 |= PWR_CR4_VBRS_Msk; // use 1.5kOhms, gives 3.02v out
PWR->CR4 |= PWR_CR4_VBE_Msk; // enable output

ok, so cap is charged by cpu internal 1k5.

so maybe you have to wait more time, until 32k osc signal "ok" .

or/and reset restart rtc , when signal "ok".

see .. about problems with rtc, when vbat was too low...

http://www.efton.sk/STM32/gotcha/index.html

 

If you feel a post has answered your question, please click "Accept as Solution".

Where you place PWR->CR4 lines? Have you enabled PWR clk before?

gbm
Principal

At register level, it should be both, LSI_ON | LSI_BYPASS, not just one of them. In CubeMX - select Bypass option for LSE

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

The PWR->CR4 lines are between the call to HAL_Init(), and the call to SystemClock_Config() which sets up the osc.

Even when the timeout is set at 10 seconds, it still times out.