cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L412CB Flash Write/Erase fails first time only, then works OK.

DBhut.1
Senior
uint32_t write_to_flash(uint8_t * buf, uint16_t length){
	if((length)>2047) return 0xFFFFFFFF;
	uint32_t base_addr=0;
	base_addr=getHexAddressPage(DATA_PAGE);
 
	uint32_t PAGEError;
 
  /* Unlock the Flash to enable the flash control register access *************/
	HAL_FLASH_Unlock();
	__HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_EOP | FLASH_FLAG_OPERR | FLASH_FLAG_PROGERR | FLASH_FLAG_WRPERR | FLASH_FLAG_PGAERR |
	  FLASH_FLAG_SIZERR | FLASH_FLAG_PGSERR | FLASH_FLAG_MISERR | FLASH_FLAG_FASTERR | FLASH_FLAG_OPTVERR);
	  __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_ALL_ERRORS);
   /* Erase the user Flash area*/
 
   /* Fill EraseInit structure*/
   EraseInitStruct.TypeErase= FLASH_TYPEERASE_PAGES;
   EraseInitStruct.Page = DATA_PAGE;
   EraseInitStruct.NbPages= 1;
 
   if (HAL_FLASHEx_Erase(&EraseInitStruct, &PAGEError) != HAL_OK)
   {
	   DBGx("Flash Erase Fail\r\n");
		 HAL_FLASH_Lock();
	   return HAL_FLASH_GetError();
   }
 
	 for (uint32_t i = 0; i < length; i += 8)
	 {
	    uint64_t data64 = u8touint64(buf+i);
	    PAGEError=HAL_FLASH_Program(FLASH_TYPEPROGRAM_DOUBLEWORD, i + base_addr, data64);
	    if (PAGEError != HAL_OK)
	    {
	      HAL_FLASH_Lock();
	      DBGx("2 IS_FLASH_PAGE(Page):%d at mem:%x,PAGEError:%x\r\n",IS_FLASH_PAGE(DATA_PAGE),DATA_PAGE,PAGEError);
	      return PAGEError;
	    }
	 }
 
	HAL_FLASH_Lock();
	DBGx("Flash Error:%d\r\n",PAGEError);
	return PAGEError;
}

Above code is used to write flash

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Kamil Duljas
Senior III

Which line return error?​

Dudo
DBhut.1
Senior

At line 20, Flash Erase Fail.

KDJEM.1
ST Employee

Hello @DBhut.1​ ,

Could you please check the BankNumber, FirstPage, and NbOfPages.

For that, I recommend you to get inspired from the available FLASH_EraseProgram example in STM32CubeL4 package.

I hope this help you!

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

DBhut.1
Senior

There is no page issue, as Flash work after first time erase fail, and working fine since 5 months. Only issue is After upload code to fresh MCU, and perform Flash Write, It fails, and we have to perform operation again. So, there may be issue with code or something else, which prevents, Flash to erase, after 1st time only.

KDJEM.1
ST Employee

Hello @DBhut.1​ ,

Thank you for this clarification.

Do you have the same issue when you using the ST example?

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

waclawek.jan
Super User

> After upload code to fresh MCU

How do you do that, exactly?

Do you power-down/power-up after finishing code uploading to the mcu?

JW

There's another error bit you're not clearing.

Instrument code so you know initial register states and WHY the Erase reportedly fails.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I will try thanks

No, I don't do any Powerup/down, just flash the code, and write my configuration default values of data to flash, for future use.