cancel
Showing results for 
Search instead for 
Did you mean: 

PS/2 Trackball Integration Issues on STM32F072

vuckale
Associate

Hey all,

I’m working on integrating a PS/2 trackball into a custom PCB using QMK, and I’ve hit a weird snag. My MCU is an STM32F072 (custom PCB, project repo here: https://github.com/vuckale/takt11800/tree/master/Firmware. I’m following the official https://docs.qmk.fm/features/ps2_mouse and using the “interrupt” version for the mouse interface.

Here’s the issue:

- Sometimes after flashing, the trackball works perfectly.

- If I unplug and plug the keyboard back into the PC, the trackball usually stops working. Sometimes after multiple re-plugs or after waiting a while, it comes back, but it’s super inconsistent.

I’ve tried:

- Different pin combos for clock/data (B3/A15, A0/A1, B10/B11)—all with 4.7k pull-ups to 5V except A0/A1 which are not 5V tolerant and I pull them up with 10k resistors to 3.3V.

- If I add #define PS2_MOUSE_USE_REMOTE_MODE in config.h, then the trackball is detected every time after replug… but the cursor goes crazy—jumps around the screen, and left/right click events randomly fire by themselves.

What’s really odd:

I’ve implemented almost the same code on a Blackpill STM32 (STM32F103) https://github.com/vuckale/compaq_mx_11800_qmk_via/tree/main/handwired and it works perfectly every time with the same kind of trackball.

Would love any troubleshooting tips, especially from anyone who’s gotten a QMK PS/2 mouse reliably working on STM32F0 series. I know this might not be the best place to ask since it’s pretty technical, but the folks at the QMK forums haven’t been able to help, and at this point I suspect it might be more of a hardware/electrical issue than just firmware. Any ideas are welcome!

Thanks in advance!

Trackball in question:  https://imgur.com/a/Ejsuc9h

1 REPLY 1
Andrew Neil
Super User

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

 


@vuckale wrote:

using QMK,


You mean this: https://qmk.fm/ ?

That's not an ST thing, so have you asked on their forum?

https://docs.qmk.fm/support

EDIT: Sorry - missed that you had done that.

 


@vuckale wrote:

 If I unplug and plug the keyboard back into the PC,


What keyboard? What PC?

Please give some more details of your setup - how do these things all fit together?

 


@vuckale wrote:

the trackball usually stops working.


Please give more details of this "stops working" case.

  • What are you expecting it to do?
  • What is it actually doing?
  • Is the problem with the trackball itself, or your STM32?
  • What testing/investigation/debugging have you done to find what's going on?

@vuckale wrote:

Trackball in question:  https://imgur.com/a/Ejsuc9h


You can post photos directly here - no need for 3rd-party sites

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.