2017-09-20 04:47 AM
Hi
When STM32L4 Plus series will be available to buy?
Any datasheets yet?
2017-11-15 11:14 AM
Have a look at Mouser 423-G1120TB103GF
2017-11-15 11:44 AM
Not a low cost screen then... ST must be getting a better price
Arrow has DISCO boards, quoting $125, Mouser says they have delivery tomorrow quoting $89
https://www.mouser.com/ProductDetail/STMicroelectronics/STM32L4R9I-DISCO
2017-11-15 12:00 PM
2017-11-15 12:01 PM
I'd say the $89 is introductory price and it will be up to that $125 when the first batch sells out - this is how it was with the 'F723 DISCO.
Surely the sales chain pumps up the price of the displays quite significantly.
JW
2017-11-15 12:05 PM
Yeah that'd be very nice but this is a really tiny, watch-sized display...
2017-11-15 12:05 PM
Arrow had 10, Mouser 20, so not stocking deeply..
2017-11-15 12:27 PM
Wow Uwe, thanks.
Ugh, the price is... I may buy a DiscoL4+, keep the display and throw the rest away... 😉
Jan
2017-11-16 08:46 AM
L4 with 120MHZ is very good, it increase the range of applications. But it would be much better if it had kept the 3xADC, 2xCAN and 64 pins options. I would give up SRAM3 and OCTASPI for that.
Ari.
2017-11-16 12:44 PM
My expectation is that there are likely instrumentation sized ones, not just stuff left over from failed watch or mediaplayer products. I don't think Apple would get out of bed for this resolution, so got to think there are bigger and more competitive displays in this format.
I'd take the boards, most of my stuff is headless...
I'm assuming these are going to be plug in compatible with ST's previous LCD connectors..
2017-11-16 12:48 PM
They are quite impressive at 150 MHz, especially in a 32 pin package.
If I were ST I'd requalify the earlier parts in high speed bands, the design seems to have significant headroom.