2017-09-20 4:47 AM
Hi
When STM32L4 Plus series will be available to buy?
Any datasheets yet?
2017-09-20 8:18 AM
Hello,
Thanks for your interest on our future STM32 products.
It will be announced and available mid of November.
If you need to know more in between I suggest you to contact your STMicroelectronics contact or distributor.
Regards,
Bertrand
2017-09-26 6:56 AM
stcube already provides device headers. With a 'diff' you can see the differences...
2017-10-03 7:17 PM
Found some info about it at the end of this presentation:
2017-10-04 10:34 AM
Current L4 parts run north of 150 MHz, 120 MHz is hardly a stretch...
2017-10-06 9:04 AM
Current L4 parts run north of 150 MHz
Which?
JW
2017-10-06 9:44 AM
On the bench the L476RG topped out at 158 MHz, the L496ZG somewhat below, they both perform solidly at 140 MHz.
Both have 3-bit wait state counter, so primary constraint is ART/prefetch path.
The 120 MHz number is probably with 60 MHz APB
2017-10-06 10:12 AM
They may be artificially underrated by ST to create room for step-up, or because testing for higher frequencies might be too expensive, or any other reason - but I tend to stick to the DS values for the stuff we sell.
JW
2017-10-06 12:56 PM
No doubt, this was more of an intellectual exercise to see how much headroom there was in the design. Figuring more advantageous design than the original F2/F4, better process, and peripheral buses now running at 100-108 MHz in some of the designs.
The Cortex-M0(+) parts can also run faster than advertised, but with limited flash wait state options, pll settings, and no cache/prefetch as speed ramps above 28 MHz the speed of the flash becomes dominant.
2017-10-25 2:23 PM
L432KC topped out at 150 MHz