2017-04-07 1:27 AM
Hello everybody,
I have the following situation:
My question now is:
What I found out so far:
2017-04-07 1:29 AM
Pardon me for the bad manners - I pressed Enter to soon. Here is the proper ending of my post:
Hope you can help me with my problem.
Kind regards
Markus
2017-04-07 2:04 AM
For the 'L4 DMA, probably AN2548 is appropriate, even if it talks about F1/L1 - I believe the DMA in 'L4 is the same/similar than that in 'F1/'L1/'F0/'L0 (and quite different from that found in 'F2/'F4/'F7). However, the total transfer time calculation is not trivial and in your case might be quite different from what's given there, as:
- there may be simpler/shorter arbitration within the DMA if only one channel is used
- there may be simpler/shorter arbitration on the AHB/APB bridge if the AHB/APB clock is 1:1
- there may be simpler/shorter arbitration on the bus matrix if processor won't access the shared resources (SRAM, APB) ever
It may quite well be that you've already found the sweet spot.
JW