2019-06-18 6:41 AM
Hi sir,
I ask a question about optionbytes nBFB2 of STM32L151VE.
I checked User Manual and wanted to confirm some information about nBFB2.
1) Option byte register (FLASH_OBR) : bit nBFB2 default value = 1 , see attached file optionbytes_1.png
2) Option byte memory address 0x1FF8 0004H : read bit7 = BFB2 value, but there is no default value describtion about this bit.
My question:
1) Which default value is nBFB2 ? 0 or 1 ?
2) If user read address 0x1FF8 0004H to get bit7(nBFB2) = 0, then try to write 1 using FLASH_OB_BORConfig(), MCU should does a reset behavior , right?
After MCU reset, then read this address again, user should get bit7(nBFB2) = 1, then code execute users app code.
Is my understanding right or not? If right, where i could get this information description on ST spec? Would you mind give me the link?
Thanks a lot and hope your help ASAP.
Best Regards,
Vincent
2024-04-27 10:09 AM
I'm having the same issue.STM32L151RET6,nBFB2,default value maybe is 1, but some is 0, so the mcu reset and rest.