cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32h753zi uart error handler

A3
Associate III

Hi,

When HAL_Uart_errorhandler is triggered, how can we check if the trigger is for reception or transmission?

4 REPLIES 4
Andrew Neil
Super User

Check the UART error & status flags - each one will be applicable to only receive or transmit.

eg, you can't get framing or parity errors on transmit - only receive!

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Possible UART errors listed below, and which one is for TX, and which one is for RX mentioned below. Please let me know if my understandings are correct.

#define HAL_UART_ERROR_NONE (0x00000000U) /*!< No error */
#define HAL_UART_ERROR_PE (0x00000001U) /*!< Parity error */
#define HAL_UART_ERROR_NE (0x00000002U) /*!< Noise error */
#define HAL_UART_ERROR_FE (0x00000004U) /*!< Frame error */
#define HAL_UART_ERROR_ORE (0x00000008U) /*!< Overrun error */
#define HAL_UART_ERROR_DMA (0x00000010U) /*!< DMA transfer error */
#define HAL_UART_ERROR_RTO (0x00000020U) /*!< Receiver Timeout error */


Receive Error: HAL_UART_ERROR_PE, HAL_UART_ERROR_FE, HAL_UART_ERROR_NE, HAL_UART_ERROR_ORE, HAL_UART_ERROR_RTO, HAL_UART_ERROR_DMA
Transmit Error: HAL_UART_ERROR_DMA

Look-up the definitions of those bits in the Reference Manual.

These, by definition,  can only happen on receive:

#define HAL_UART_ERROR_PE (0x00000001U) /*!< Parity error */ #define HAL_UART_ERROR_NE (0x00000002U) /*!< Noise error */ #define HAL_UART_ERROR_FE (0x00000004U) /*!< Frame error */ #define HAL_UART_ERROR_RTO (0x00000020U) /*!< Receiver Timeout error */

 

 These you'd have to check in the Refence Manual:

#define HAL_UART_ERROR_ORE (0x00000008U) /*!< Overrun error */ #define HAL_UART_ERROR_DMA (0x00000010U) /*!< DMA transfer error */

 

Note How to insert source code.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
Super User

> Please let me know if my understandings are correct.

These are correct.

If you feel a post has answered your question, please click "Accept as Solution".