2025-02-18 6:04 AM
Good afternoon,
I have a question regarding the best strategy to follow on how to measure multiple channels with the ADC (triggered with timer) and map them to the DMA.
I have followed the project called ADC_DMA_Transfer that can be found in the Project's folder of the U575 family and it works and i can see in my buffer the 5 values of the ADC that i want to monitor in continuous conversion mode. However this solution creates an ADCQueue and an ADCNode (I do not really know what it is).
/* USER CODE BEGIN 2 */
MX_ADCQueue_Config();
__HAL_LINKDMA(&hadc4, DMA_Handle, handle_GPDMA1_Channel10);
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel10, &ADCQueue) != HAL_OK)
{
Error_Handler();
}
if (HAL_ADC_Start_DMA(&hadc4, (uint32_t *)aADCxConvertedData, (ADC_CONVERTED_DATA_BUFFER_SIZE) ) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(&hadc4, DMA_Handle, handle_GPDMA1_Channel3);
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel3, &ADCQueue) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(&hadc4, DMA_Handle, handle_GPDMA1_Channel4);
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel4, &ADCQueue) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(&hadc4, DMA_Handle, handle_GPDMA1_Channel9);
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel9, &ADCQueue) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(&hadc4, DMA_Handle, handle_GPDMA1_Channel11);
if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel11, &ADCQueue) != HAL_OK)
{
Error_Handler();
}I do not really know how to implement the timer2 to trigger the ADC but i have found the following video https://www.youtube.com/watch?v=pLsAhJ8umJk in which is not using the strategy that can be found on the projects of the U575 family.
Why this two different approaches? Can i implement my solution with both projects?
Thank you,
Marc
2025-02-18 6:56 AM
Hello @Marc3,
>>However this solution creates an ADCQueue and an ADCNode (I do not really know what it is).
This involves creating a queue of DMA requests and linking them to the ADC handle, you can check this article:
How to configure the linked list mode in STM32Cube... - STMicroelectronics Community
>>I do not really know how to implement the timer2 to trigger the ADC
You can start with this hands-on:
Hands-On with STM32 Timers: Trigger Periodic ADC Conversions
Using Timers to Trigger ADC conversions periodical... - STMicroelectronics Community
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.