2025-01-22 1:04 AM
Hi, I have problem. I have idea: my STM32H745 must read GPIO state as quickly as possible. FCPU = ~400MHz
I wrote the program in assembler for M7
LED_ON()
ldr r2, [r3, #IDR]
ldr r2, [r3, #IDR]
... ~650x
LED_OFF()
...
only read, IDR, no write (no record yet)
And when I measure with an oscilloscope the led output is on for 25us -> one LDR 15 cycles clock CPU. When I read from RAM it takes about 12us, but GPIO 25us.
This is too slow for me. I tried all the tricks and combinations of LDR; STR ... LDR LDR STR STR ... LDR AND LDR STR AND ... Minimum is 25us.
LDR gpio and STR ram are without comment at all. Some astronomical values come out that can be obtained from AVR or DSPIC.
I tried FMC to read and it was even worse.
What is the fastest way to read the state of a ~40MHz pin?
Solved! Go to Solution.
2025-01-22 1:29 AM - edited 2025-01-22 1:30 AM
Two possibilities:
- For single pin - use SPI MISO line and SPI RX DMA. This guarantees fixed sampling frequency.
- For multiple pins - use timer-triggered DMA from port to memory. Some frequency variations and jitter will appear.
2025-01-22 1:29 AM - edited 2025-01-22 1:30 AM
Two possibilities:
- For single pin - use SPI MISO line and SPI RX DMA. This guarantees fixed sampling frequency.
- For multiple pins - use timer-triggered DMA from port to memory. Some frequency variations and jitter will appear.
2025-01-30 11:22 AM
Ok works. It's a pity that it can't be done differently. Creating a 30-40MHz real-time system with non-standard pin analysis is practically impossible with ARM :(. Too large a range of possible problems. My system worked somehow, but it was supposed to be very easy, but it was very confusing and I probably won't come up with such an idea again :)
2025-01-30 12:14 PM
If you talk about the direct r/w to a port/pin, its not "ARM" making it fast or slow - its how the SOC is built and connected to the core.
So on H7 you more on a "PC" , fast core and calculations, but gpio is "far away" from the core, going over some bus connections to reach a port.
If you want direct r/w to a port/pin fast, look at the M33-core series, maybe stm32H563 .
Here ports are on direct connection to core, so you get : (in my tests)
(speed test, option -O2 , at 250MHz core ) bsrr 4ns ; so port access here 1 cyc, 4 ns.
2025-01-31 12:41 AM
I'll try it sometime.
I saw that it's a long way from the core to GPIO, but I didn't think it was that far :). And the documentation doesn't have many details about it, so it just came out that way.