cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H745: DS and RM disagree, which to believe?

Mike Ciholas
Associate III

STM32H745 datasheet says:

RTC_OUT can come out PB2 port. No other port is listed in the DS for RTC_OUT. See table 8, page 62. RTC_OUT also listed in table 10, page 90, and note for PC13, page 92.

STM32H745 reference manual says:

RTC_OUT can be directed to PC13 or PB2, with PB2 not being useful in standby/VBAT modes. See table 387, page 2081.

Okay, so which document is correct?

My instincts say the RM likely is correct, but building PCBs based on instinct will end up costing you someday, so I want the documents to be clear and consistent.

10 REPLIES 10

Follow-up thread: STM32H745: DS and RM misalignment: doc update required

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.