2025-03-18 12:39 AM
Hello there!
I've designed a board based on the STM32H743Zit Nucleo board, but unfortunately, I'm facing difficulties with the USB functionality. I'm unsure if it's a matter of configuration or firmware. When I tested USB settings and functionality using the Nucleo board, everything worked seamlessly. but in my costom board its not working and i donot have com port
2025-03-18 1:29 AM
Hello @kmh011 and welcome to the community,
If it was the same firmware tested on both boards (custom / Nucleo), most probably it's a hardware issue.
You need to share your schematics so others can help you efficiently.
2025-03-18 1:33 AM - edited 2025-03-18 5:48 AM