cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 with USB C connector

kmh011
Associate II

Hello there!

I've designed a board based on the STM32H743Zit Nucleo board, but unfortunately, I'm facing difficulties with the USB functionality. I'm unsure if it's a matter of configuration or firmware. When I tested USB settings and functionality using the Nucleo board, everything worked seamlessly. but in my costom board its not working and i donot have com port

2 REPLIES 2
mƎALLEm
ST Employee

Hello @kmh011 and welcome to the community,

If it was the same firmware tested on both boards (custom / Nucleo), most probably it's a hardware issue.

You need to share your schematics so others can help you efficiently.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.