cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H745I-DISCO integrated st-linkv3 not working

RafaelS
Associate III

Hello,

I am working in STM32H745I-DISCO since January. Yesterday I have disconected the USB of CN14 connector ( I used it for programming/debuging and powering). This morning I have connected de USB but the board doesn´t work. After test de voltages I have realised that the st-linkc3 does not pull up the pin T_PWR_EN of component U24.

I have tried to connect through stm32cubeprogramer but Error: no debug probe detected appears.

There are any way to recover this?

Thank you in advance.

 

1 ACCEPTED SOLUTION

Accepted Solutions

Thanks for the quick response. And sorry for my English.

I meant that I disconnected the USB cable from the CN14 connector.

 

It finally seemed to be a problem with the computer. When I checked in Device Manager to see if the connection with the ST-Link was present, I realized that Device Manager was not responding, and I couldn't close it. I restarted the computer, and now I was able to connect to the board and program it.

Best regards!

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

What do you mean by:


@RafaelS wrote:

I have disconected the USB of CN14 connector 


You've unsoldered the USB connector?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Andrew Neil
Super User

Sounds like the connector's broken?

Have you tried powering the board through any of the other options?

AndrewNeil_0-1742291192727.png

https://www.st.com/resource/en/user_manual/um2488-discovery-kits-with-stm32h745xi-and-stm32h750xb-mcus-stmicroelectronics.pdf#page=11

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Thanks for the quick response. And sorry for my English.

I meant that I disconnected the USB cable from the CN14 connector.

 

It finally seemed to be a problem with the computer. When I checked in Device Manager to see if the connection with the ST-Link was present, I realized that Device Manager was not responding, and I couldn't close it. I restarted the computer, and now I was able to connect to the board and program it.

Best regards!