cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h723zg Clause 45 MDIO

heisenbug
Associate III

Hi all,

i see H7 supports clause 45 MDIO access, but in the HAL library looks not implemented, i see only clause 22.

How should i proceed to read/write c45 ?

 Thanks,

angelo

4 REPLIES 4
SofLit
ST Employee

Hello,

Which MDIO interface you are talking about? is it the MDIO of the ETH or the MDIO slave (MDIOS)?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
heisenbug
Associate III

MDIO inside the ETH IP

heisenbug
Associate III

Well, found now that the PHY chip i am using is supporting C22 to C45 bridge (multiple devices addressing), so don't need to add Clause 45 to HAL. Anyway, since h7 supports Clause 45, would be nice to have it imnplemented in HAL.  

SofLit
ST Employee

Hello,

Internal ticket already raised for follow-up 177202

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.