cancel
Showing results for 
Search instead for 
Did you mean: 

stm32h723zg Clause 45 MDIO

heisenbug
Associate III

Hi all,

i see H7 supports clause 45 MDIO access, but in the HAL library looks not implemented, i see only clause 22.

How should i proceed to read/write c45 ?

 Thanks,

angelo

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

I've got a feedback regarding that request. The decision was not to add Clause45 support for the actual product including H7 for many reason including the fact that there is no ST STM32 development kits is equipped with a Clause45-capable PHY. But Clause45 (maybe) it will be addressed in the HAL of newer products.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

5 REPLIES 5
mƎALLEm
ST Employee

Hello,

Which MDIO interface you are talking about? is it the MDIO of the ETH or the MDIO slave (MDIOS)?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
heisenbug
Associate III

MDIO inside the ETH IP

heisenbug
Associate III

Well, found now that the PHY chip i am using is supporting C22 to C45 bridge (multiple devices addressing), so don't need to add Clause 45 to HAL. Anyway, since h7 supports Clause 45, would be nice to have it imnplemented in HAL.  

mƎALLEm
ST Employee

Hello,

Internal ticket already raised for follow-up 177202

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

Hello,

I've got a feedback regarding that request. The decision was not to add Clause45 support for the actual product including H7 for many reason including the fact that there is no ST STM32 development kits is equipped with a Clause45-capable PHY. But Clause45 (maybe) it will be addressed in the HAL of newer products.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.