cancel
Showing results for 
Search instead for 
Did you mean: 

MDIO access network switch

ranran
Senior II

Hello,

I hope someone will have an idea for the following:

I use marvell switch mv88e6071 with stm32h7.

The switch works with MDIO, clause 22.

I managed to read switch identifies (0x715) when using phy address 0x18.

But the switch expects to read switch identifier (as well as other registers) only if phy_address (=port in switch) is between 8 to 0xE, while I succeed in reading only if I use phy address = 0x18 and 0x19.

It seems that routine HAL_ETH_ReadPhyRegister is using clause 22, (and not clause 45), and this is correct.

I have not yet checked in scope and analyzed the bits in MDIO command.

Is there anything which can explain why HAL_ETH_ReadPhyRegister does not behave as expected ? (assuming that the problem is in STM32 and not in switch)

Thanks

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0