cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 USB CDC - without VBUS pin?

Rahu2710
Associate

I am using the STM32H743ZIT6 MCU to enable USB CDC. In my schematic, I have not defined the VBUS pin; I have only defined the CDC lines. Can I still use CDC without the VBUS pin? Below is the photo of my schematic for reference. Please help me.

Thank you for your assistance.

1 REPLY 1
TDK
Guru

> Can I still use CDC without the VBUS pin?

Yes. You are not required to connect VBUS to use USB.

The USB standard does require that you check VBUS before energizing the data lines, but you can typically safely ignore that. If your device is USB powered, there is no need to check.

Schematic looks good.

If you feel a post has answered your question, please click "Accept as Solution".